EDMA3_DRV_EvtQuePriority Struct Reference
[EDMA3 Driver Data Structures]

Event queue priorities setup. More...

#include <edma3_drv.h>

Data Fields

unsigned int evtQPri [EDMA3_MAX_EVT_QUE]
 Event Queue Priorities.

Detailed Description

Event queue priorities setup.

It allows to change the priority of the individual queues and the priority of the transfer request (TR) associated with the events queued in the queue.


The documentation for this struct was generated from the following file:

Generated on Fri Jan 28 15:45:39 2011 for EDMA3 Driver by  doxygen 1.6.1