EDMA3_RM_ResDesc Struct Reference
[EDMA3 Resource Manager Data Structures]

Handle to a Resource. More...

#include <edma3_rm.h>


Data Fields

unsigned int resId
EDMA3_RM_ResType type


Detailed Description

Handle to a Resource.

Field Documentation

Resource Id Range of resId values : As an example, for resource Type = EDMA3_RM_RES_DMA_CHANNEL, resId can take values from 0 to EDMA3_MAX_DMA_CH Or resId can take the value EDMA3_RM_RES_ANY.

Resource Type


The documentation for this struct was generated from the following file:

Generated on Wed Apr 7 12:02:44 2010 for EDMA3 Resource Manager by  doxygen 1.5.5