![]() |
![]() |
XDAIS
dais-x04
|
Defines the creation time parameters for all IVIDENC2 instance objects. More...
#include <ividenc2.h>
Defines the creation time parameters for all IVIDENC2 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. XDAS_Int32 IVIDENC2_Params::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDENC2_Params::encodingPreset |
Encoding preset.
XDAS_Int32 IVIDENC2_Params::rateControlPreset |
Video rate control presets.
XDAS_Int32 IVIDENC2_Params::maxHeight |
Maximum video height in pixels.
XDAS_Int32 IVIDENC2_Params::maxWidth |
Maximum video width in pixels.
XDAS_Int32 IVIDENC2_Params::dataEndianness |
Endianness of output data.
XDAS_Int32 IVIDENC2_Params::maxInterFrameInterval |
I to P frame distance. e.g. = 1 if no B frames, 2 to insert one B frame.
XDAS_Int32 IVIDENC2_Params::maxBitRate |
Maximum Bit-rate for encoding in bits per second
XDAS_Int32 IVIDENC2_Params::minBitRate |
Minumum Bit-rate for encoding in bits per second
XDAS_Int32 IVIDENC2_Params::inputChromaFormat |
Chroma format for the input buffer.
XDAS_Int32 IVIDENC2_Params::inputContentType |
Video content type of the buffer being encoded.
XDAS_Int32 IVIDENC2_Params::operatingMode |
Video coding mode of operation.
XDAS_Int32 IVIDENC2_Params::profile |
Profile indicator of video codec
XDAS_Int32 IVIDENC2_Params::level |
Level indicator of video codec
XDAS_Int32 IVIDENC2_Params::inputDataMode |
Input data mode.
XDAS_Int32 IVIDENC2_Params::outputDataMode |
Output data mode.
XDAS_Int32 IVIDENC2_Params::numInputDataUnits |
Number of input slices/rows.
inputDataMode
, like number of slices/rows/blocks etc.inputDataMode
is set to full frame mode. XDAS_Int32 IVIDENC2_Params::numOutputDataUnits |
Number of output slices/rows.
outputDataMode
, like number of slices/rows/blocks etc.outputDataMode
is set to full frame mode. XDAS_Int32 IVIDENC2_Params::metadataType[3] |
Type of each metadata plane.