![]() |
![]() |
XDAIS
dais-x04
|
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <ividenc2.h>
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDENC2_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDENC2_DynamicParams::inputHeight |
Input frame height.
XDAS_Int32 IVIDENC2_DynamicParams::inputWidth |
Input frame width.
XDAS_Int32 IVIDENC2_DynamicParams::refFrameRate |
Reference, or input, frame rate in fps * 1000.
XDAS_Int32 IVIDENC2_DynamicParams::targetFrameRate |
Target frame rate in fps * 1000.
XDAS_Int32 IVIDENC2_DynamicParams::targetBitRate |
Target bit rate in bits per second.
XDAS_Int32 IVIDENC2_DynamicParams::intraFrameInterval |
The number of frames between two I frames. For example, 30.
XDAS_Int32 IVIDENC2_DynamicParams::generateHeader |
Encode entire access unit or only header.
XDAS_Int32 IVIDENC2_DynamicParams::captureWidth |
DEFAULT(0): use imagewidth as pitch else use given capture width for pitch provided it is greater than image width.
XDAS_Int32 IVIDENC2_DynamicParams::forceFrame |
Force the current (immediate) frame to be encoded as a specific frame type.
XDAS_Int32 IVIDENC2_DynamicParams::interFrameInterval |
Number of B frames between two reference frames; that is, the number of B frames between two P frames or I/P frames. DEFAULT(0).
XDAS_Int32 IVIDENC2_DynamicParams::mvAccuracy |
Pixel Accuracy of the motion vector
XDAS_Int32 IVIDENC2_DynamicParams::sampleAspectRatioHeight |
Sample aspect ratio: Height
XDAS_Int32 IVIDENC2_DynamicParams::sampleAspectRatioWidth |
Sample aspect ratio: Width
XDAS_Int32 IVIDENC2_DynamicParams::ignoreOutbufSizeFlag |
Flag to indicate that the application has ignored the output buffer size requirement.
ignoreOutbufSizeFlag
field to XDAS_TRUE. When this flag is set to XDAS_TRUE, the encoder shouldn't return an error even if the output buffer size is less than requested by the codec.XDM_DataSyncPutFxn IVIDENC2_DynamicParams::putDataFxn |
Optional datasync "put data" function.
XDM_DataSyncHandle IVIDENC2_DynamicParams::putDataHandle |
Datasync "put data" handle
XDM_DataSyncGetFxn IVIDENC2_DynamicParams::getDataFxn |
Datasync "get data" function.
XDM_DataSyncHandle IVIDENC2_DynamicParams::getDataHandle |
Datasync "get data" handle
getDataFxn
.XDM_DataSyncGetBufferFxn IVIDENC2_DynamicParams::getBufferFxn |
Datasync "get buffer" function.
XDM_DataSyncHandle IVIDENC2_DynamicParams::getBufferHandle |
Datasync "get buffer" handle
XDAS_Int32 IVIDENC2_DynamicParams::lateAcquireArg |
Argument used during late acquire.
lateAcquireArg
value when requesting resources (i.e. during their call to acquire() when requesting the resource).