![]() |
![]() |
XDAIS
dais-x04
|
Defines the run time output arguments for all IVIDDEC instance objects. More...
#include <ividdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | extendedError |
Extended error information. . | |
XDAS_Int32 | bytesConsumed |
XDAS_Int32 | decodedFrameType |
XDAS_Int32 | outputID |
IVIDEO_BufDesc | displayBufs |
Defines the run time output arguments for all IVIDDEC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDDEC_OutArgs::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
XDAS_Int32 IVIDDEC_OutArgs::extendedError |
Extended error information. .
XDAS_Int32 IVIDDEC_OutArgs::bytesConsumed |
Bytes consumed.
XDAS_Int32 IVIDDEC_OutArgs::decodedFrameType |
Decoded frame type. See IVIDEO_FrameType.
XDAS_Int32 IVIDDEC_OutArgs::outputID |
Output ID. Refer to comment IVIDDEC_InArgs::inputID.
IVIDEO_BufDesc IVIDDEC_OutArgs::displayBufs |
The decoder fills this structure to denote the buffer pointers for current displayable frames. In case of sequences having I & P frames only, these values are identical to outBufs passed in process().