![]() |
![]() |
XDAIS
dais-x04
|
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <ividanalytics.h>
Data Fields | |
XDAS_Int32 | size |
IVIDANALYTICS_Grid * | grid |
XDM_Date | date |
IVIDANALYTICS_Rule | rule |
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.XDAS_Int32 IVIDANALYTICS_DynamicParams::size |
Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
IVIDANALYTICS_Grid* IVIDANALYTICS_DynamicParams::grid |
New overlay grid with analytics enable mask
XDM_Date IVIDANALYTICS_DynamicParams::date |
Set the current time.
IVIDANALYTICS_Rule IVIDANALYTICS_DynamicParams::rule |
Rule associated with this command (if applicable).