Data Fields

IVIDENC2_Fxns Struct Reference
[IVIDENC2 - XDM Video Encoder Interface]

Defines all of the operations on IVIDENC2 objects. More...

#include <ividenc2.h>

Collaboration diagram for IVIDENC2_Fxns:
Collaboration graph
[legend]

Data Fields

IALG_Fxns ialg
XDAS_Int32(* process )(IVIDENC2_Handle handle, IVIDEO2_BufDesc *inBufs, XDM2_BufDesc *outBufs, IVIDENC2_InArgs *inArgs, IVIDENC2_OutArgs *outArgs)
 Basic video encoding call.
XDAS_Int32(* control )(IVIDENC2_Handle handle, IVIDENC2_Cmd id, IVIDENC2_DynamicParams *params, IVIDENC2_Status *status)
 Control behavior of an algorithm.

Detailed Description

Defines all of the operations on IVIDENC2 objects.


Field Documentation

XDAIS algorithm interface.

See also:
IALG_Fxns

Basic video encoding call.

Parameters:
[in]handleHandle to an algorithm instance.
[in,out]inBufsInput video buffer descriptors.
[in,out]outBufsOutput buffer descriptors. The algorithm may modify the output buffer pointers.
[in]inArgsInput arguments. This is a required parameter.
[out]outArgsOuput results. This is a required parameter.
Remarks:
process() is a blocking call. When process() returns, the algorithm's processing is complete.
Precondition:
inBufs must not be NULL, and must point to a valid IVIDEO2_BufDesc structure.
inBufs->numPlanes will indicate the total number of input buffers supplied for input frame in the inBufs->planeDesc[] array.
inBufs->numMetaPlanes will indicate the total number of input buffers supplied for meta data planes in the inBufs->metadataPlaneDesc[] array.
outBufs must not be NULL, and must point to a valid XDM2_BufDesc structure.
outBufs->buf[0] must not be NULL, and must point to a valid buffer of data that is at least outBufs->bufSizes[0] bytes in length.
inArgs must not be NULL, and must point to a valid IVIDENC2_InArgs structure.
outArgs must not be NULL, and must point to a valid IVIDENC2_OutArgs structure.
The buffers in inBuf and outBuf are physically contiguous and owned by the calling application.
Postcondition:
The algorithm must not modify the contents of inArgs.
The algorithm must not modify the contents of inBufs, with the exception of inBufs.bufDesc[].accessMask. That is, the data and buffers pointed to by these parameters must be treated as read-only.
The algorithm must appropriately set/clear the IVIDEO2_BufDesc.planeDesc[].accessMask and IVIDEO2_BufDesc.metadataPlaneDesc[].accessMask fields in inBufs to indicate the mode in which each of the respective buffers were read. For example, if the algorithm only read from inBufs.planeDesc[0].buf using the algorithm processor, it could utilize XDM_SETACCESSMODE_READ to update the appropriate accessMask fields. The application may utilize these returned values to appropriately manage cache.
The buffers in inBufs are owned by the calling application.
Return values:
IVIDENC2_EOK

Success.

IVIDENC2_EFAIL

General failure.

See IVIDENC2_Status.extendedError for more detailed further error conditions.
IVIDENC2_EUNSUPPORTED

Request is unsupported.

Todo:
Need to review these comments. Not sure inBufs and outBufs are correctly described.

Control behavior of an algorithm.

Parameters:
[in]handleHandle to an algorithm instance.
[in]idCommand id. See XDM_CmdId.
[in]paramsDynamic parameters. This is a required parameter.
[out]statusOutput results. This is a required parameter.
Precondition:
handle must be a valid algorithm instance handle.
params must not be NULL, and must point to a valid IVIDENC2_DynamicParams structure.
status must not be NULL, and must point to a valid IVIDENC2_Status structure.
If a buffer is provided in the status->data field, it must be physically contiguous and owned by the calling application.
Postcondition:
The algorithm must not modify the contents of params. That is, the data pointed to by this parameter must be treated as read-only.
If a buffer was provided in the status->data field, it is owned by the calling application.
Return values:
IVIDENC2_EOK

Success.

IVIDENC2_EFAIL

General failure.

See IVIDENC2_Status.extendedError for more detailed further error conditions.
IVIDENC2_EUNSUPPORTED

Request is unsupported.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated