Data Fields

IAUDDEC_Status Struct Reference
[IAUDDEC - XDM Audio Decoder Interface]

Defines instance status parameters (read-only). More...

#include <iauddec.h>

Collaboration diagram for IAUDDEC_Status:
Collaboration graph
[legend]

Data Fields

XDAS_Int32 size
XDAS_Int32 extendedError
XDAS_Int32 bitRate
XDAS_Int32 sampleRate
XDAS_Int32 numChannels
XDAS_Int32 numLFEChannels
XDAS_Int32 outputFormat
XDAS_Int32 autoPosition
XDAS_Int32 fastFwdLen
XDAS_Int32 frameLen
XDAS_Int32 outputBitsPerSample
XDM_AlgBufInfo bufInfo

Detailed Description

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDDEC_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Extended error information.

Remarks:
When an internal error occurs, the algorithm will return an error return value (e.g. EFAIL, EUNSUPPORTED)
The value of each enum is the bit which is set.
Bits 31-16 are reserved. Bits 7-0 are codec and implementation specific.
The algorithm can set multiple bits to 1 based on conditions. e.g. it will set bits XDM_FATALERROR (fatal) and XDM_UNSUPPORTEDPARAM (unsupported params) in case of unsupported run time parameters.
This enumeration data type should not be used for storage, but rather only for its constant values.
See also:
XDM_ErrorBit

Average bit rate, in bits per second.

Sampling frequency, in Hz. For example, if the sampling frequency is 44.1 kHz, this field will be 44100.

Number of Channels. See IAUDIO_ChannelId.

Number of LFE (Low Frequency Effects) channels in the stream.

The output PCM format. See IAUDIO_PcmFormat.

Flag to indicate support for random position decoding, which means that a stream can be decoded from any point. 0 indicates this feature is not supported, 1 indicates this feature is supported.

Recommended fast forward length in bytes in case of random position decoding.

Number of samples decoded per process() call.

Number of bits per output sample. For example, if the value of the field is 16, there are 16 output bits per PCM sample.

Input and output buffer information. See XDM_AlgBufInfo.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated