![]() |
![]() |
|
TI-RTOS Drivers
tidrivers_full_2_21_01_01
|
|
Macros | |
| #define | SDHostCC3200_STATUS_SUCCESS (0) |
| Successful status code returned by SDHostCC3200_control(). More... | |
| #define | SDHostCC3200_STATUS_ERROR (-1) |
| Generic error status code returned by SDHostCC3200_control(). More... | |
| #define | SDHostCC3200_STATUS_UNDEFINEDCMD (-2) |
| An error status code returned by SDHostCC3200_control() for undefined command codes. More... | |
| #define | SDSPI_STATUS_SUCCESS 0 |
| Successful status code returned by SDSPI_control(). More... | |
| #define | SDSPI_STATUS_ERROR -1 |
| Generic error status code returned by SDSPI_control(). More... | |
| #define | SDSPI_STATUS_UNDEFINEDCMD -2 |
| An error status code returned by SDSPI_control() for undefined command codes. More... | |
SDSPI_STATUS_* macros are general status codes returned by SDSPI_control()
SDSPICC3200_STATUS_* macros are command codes only defined in the SDSPICC3200.h driver implementation and need to:
SDSPIEUSCIA_STATUS_* macros are command codes only defined in the SDSPIEUSCIA.h driver implementation and need to:
SDSPIEUSCIB_STATUS_* macros are command codes only defined in the SDSPIEUSCIB.h driver implementation and need to:
SDSPIMSP432_STATUS_* macros are command codes only defined in the SDSPIMSP432.h driver implementation and need to:
SDSPITiva_STATUS_* macros are command codes only defined in the SDSPITiva.h driver implementation and need to:
SDSPIUSCIA_STATUS_* macros are command codes only defined in the SDSPIUSCIA.h driver implementation and need to:
SDSPIUSCIB_STATUS_* macros are command codes only defined in the SDSPIUSCIB.h driver implementation and need to:
| #define SDHostCC3200_STATUS_SUCCESS (0) |
Successful status code returned by SDHostCC3200_control().
SDSPI_control() returns SDSPI_STATUS_SUCCESS if the control code was executed successfully.
Note: This status code is also used internally in the driver to indicate that a command sent to the SD card was successful.
| #define SDHostCC3200_STATUS_ERROR (-1) |
Generic error status code returned by SDHostCC3200_control().
SDHostCC3200_control() returns SDHostCC3200_STATUS_ERROR if the control code was not executed successfully.
Note: This status code is also used internally in the driver to indicate if a command sent to the SD card succeeded.
| #define SDHostCC3200_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by SDHostCC3200_control() for undefined command codes.
SDHostCC3200_control() returns SDHostCC3200_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.
| #define SDSPI_STATUS_SUCCESS 0 |
Successful status code returned by SDSPI_control().
SDSPI_control() returns SDSPI_STATUS_SUCCESS if the control code was executed successfully.
| #define SDSPI_STATUS_ERROR -1 |
Generic error status code returned by SDSPI_control().
SDSPI_control() returns SDSPI_STATUS_ERROR if the control code was not executed successfully.
| #define SDSPI_STATUS_UNDEFINEDCMD -2 |
An error status code returned by SDSPI_control() for undefined command codes.
SDSPI_control() returns SDSPI_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.