![]() |
![]() |
|
TI-RTOS Drivers
tidrivers_full_2_21_01_01
|
| ADC.h | ADC driver interface |
| ADCBuf.h | ADCBuf driver interface |
| ADCBufCC26XX.h | ADCBuf driver implementation for a CC26XX analog-to-digital converter |
| ADCCC26XX.h | ADC driver implementation for the ADC peripheral on CC26XX |
| ADCMSP432.h | ADC driver implementation for the ADC peripheral on MSP432 |
| buzzer.h | PWM-based buzzer interface |
| Camera.h | Camera driver interface |
| CameraCC3200DMA.h | Camera driver implementation for a CC3200 Camera controller |
| ClockP.h | Clock interface for the RTOS Porting Interface |
| Codec1.h | Implementation of TI Codec Type 1 (IMA ADPCM) encoding and decoding |
| CryptoCC26XX.h | Crypto driver implementation for a CC26XX Crypto controller |
| DebugP.h | Debug support |
| diskio.h | |
| Display.h | Generic interface for text output |
| DisplayDogm1286.h | |
| DisplayExt.h | Extention of Display to access GrLib functionality in capable displays |
| DisplayLog.h | |
| DisplaySharp.h | |
| DisplayUart.h | |
| EMAC.h | EMAC driver interface |
| EMACSnow.h | EMACSnow Driver |
| EMACTiva.h | EMACTiva Driver |
| ExtFlash.h | External flash storage abstraction |
| ff.h | |
| ffcio.h | |
| ffconf.h | |
| fsutils.h | |
| GPIO.h | GPIO driver |
| GPIOCC26XX.h | CC26XX GPIO driver |
| GPIOCC3200.h | CC3200 GPIO driver |
| GPIOMSP430.h | MSP430 GPIO driver |
| GPIOMSP432.h | MSP432 GPIO driver |
| GPIOTiva.h | Tiva GPIO driver |
| GPTimerCC26XX.h | GPTimer driver implementation for CC26XX/CC13XX |
| grlib.h | |
| HwiP.h | Hardware Interrupt module for the RTOS Porting Interface |
| I2C.h | I2C driver interface |
| I2CCC26XX.h | I2C driver implementation for a CC26XX I2C controller |
| I2CCC3200.h | I2C driver implementation for a CC3200 I2C controller |
| I2CEUSCIB.h | I2CEUSCIB driver implementation for an EUSCIB controller |
| I2CMSP432.h | I2C driver implementation for the EUSCI controller on MSP432 |
| I2CSlave.h | I2CSlave driver interface |
| I2CSlaveMSP432.h | I2CSlave driver implementation for the EUSCI controller on MSP432 |
| I2CTiva.h | I2C driver implementation for a Tiva I2C controller |
| I2CUSCIB.h | I2CUSCIB driver implementation for a USCIB controller |
| I2S.h | I2S driver interface |
| I2SCC3200DMA.h | I2S driver implementation for a CC3200 I2S controller |
| integer.h | |
| LCDDogm1286.h | LCD driver implementation for a DOGM128W-6 LCD display |
| LCDDogm1286_util.h | |
| List.h | Linked List interface for use in drivers |
| MutexP.h | Mutex module for the RTOS Porting Interface |
| NVS.h | PRELIMINARY Non-Volatile Storage Driver |
| NVSCC26XX.h | |
| NVSCC3200.h | |
| NVSMSP432.h | |
| NVSTiva.h | |
| PDMCC26XX.h | PDM driver implementation for a CC26XX PDM controller |
| PDMCC26XX_util.h | PDM utility includes helper functions for configuring the CC26XX I2S controller |
| PIN.h | Generic PIN & GPIO driver |
| PINCC26XX.h | Device-specific pin & GPIO driver for CC26xx family [def] |
| Power.h | Power manager interface |
| PowerCC26XX.h | Power manager interface for CC26XX |
| PowerCC3200.h | Power manager interface for the CC3200 |
| PowerMSP432.h | Power manager interface for the MSP432 |
| PWM.h | PWM driver interface |
| PWMTimerCC26XX.h | PWM driver implementation for CC26XX/CC13XX |
| PWMTimerCC3200.h | PWM driver implementation using CC3200 General Purpose Timers |
| PWMTimerMSP432.h | PWM driver implementation using Timer_A peripherals |
| PWMTimerTiva.h | PWM driver implementation using Tiva General Purpose Timers |
| PWMTiva.h | PWM driver implementation for Tiva PWM peripherals |
| RF.h | RF driver for the CC26/13xx family |
| RingBuf.h | |
| SDHostCC3200.h | SDHost driver implementation for the CC3200 |
| SDSPI.h | SDSPI driver interface |
| SDSPICC3200.h | SDSPI driver implementation for a CC3200 SPI peripheral used with the SDSPI driver |
| SDSPIEUSCIA.h | SDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver |
| SDSPIEUSCIB.h | SDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver |
| SDSPIMSP432.h | SDSPI driver implementation using an EUSCI SPI peripheral for MSP432 |
| SDSPITiva.h | SDSPI driver implementation for a Tiva SPI peripheral used with the SDSPI driver |
| SDSPIUSCIA.h | SDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver |
| SDSPIUSCIB.h | SDSPI driver implementation for a USCI SPI peripheral used with the SDSPI driver |
| SemaphoreP.h | Semaphore module for the RTOS Porting Interface |
| SensorBmp280.h | Driver for the Bosch BMP280 Pressure Sensor |
| SensorHdc1000.h | Driver for Texas Instruments HCD1000 humidity sensor |
| SensorI2C.h | Simple interface to the TI-RTOS driver. Also manages switching between I2C-buses |
| SensorMpu9250.h | Driver for the InvenSense MPU9250 Motion Processing Unit |
| SensorOpt3001.h | Driver for the Texas Instruments OPT3001 Optical Sensor |
| SensorTagTest.h | Test code for SensorTag |
| SensorTmp007.h | Driver for the Texas Instruments TMP007 infra-red thermopile sensor |
| SensorUtil.h | Common utility code for SensorTag |
| SharpGrLib.h | |
| SPI.h | SPI driver interface |
| SPICC26XXDMA.h | SPI driver implementation for a CC26XX SPI controller using the UDMA controller |
| SPICC3200DMA.h | SPI driver implementation for a CC3200 SPI controller using the micro DMA controller |
| SPIEUSCIADMA.h | SPI driver implementation for a USCIA peripheral using the micro DMA controller |
| SPIEUSCIBDMA.h | SPI driver implementation for a USCIB peripheral using the micro DMA controller |
| SPIMSP432DMA.h | SPI driver implementation for a EUSCI peripheral on MSP432 using the micro DMA controller |
| SPITivaDMA.h | SPI driver implementation for a TivaSPIcontroller using the micro DMA controller |
| SPIUSCIADMA.h | SPI driver implementation for a USCIA peripheral using the micro DMA controller |
| SPIUSCIBDMA.h | SPI driver implementation for a USCIB peripheral using the micro DMA controller |
| tirtos_config.h | |
| UART.h | UART driver interface |
| UARTCC26XX.h | UART driver implementation for a CC26XX UART controller |
| UARTCC3200.h | UART driver implementation for a CC3200 UART controller |
| UARTCC3200DMA.h | UART driver implementation for a CC3200 UART controller, using the micro DMA controller |
| UARTEUSCIA.h | UART driver implementation for a EUSCIA peripheral |
| UARTMSP432.h | UART driver implementation for a EUSCIA peripheral for MSP432 |
| UARTTiva.h | UART driver implementation for a Tiva UART controller |
| UARTTivaDMA.h | UART driver implementation for a Tiva UART controller thay uses DMA |
| UARTUSCIA.h | UART driver implementation for a USCIA peripheral |
| UDMACC26XX.h | UDMACC26XX driver implementation |
| UDMACC3200.h | UDMA driver implementation for CC3200 |
| UDMAMSP432.h | UDMA driver implementation for MSP432 |
| USBMSCHFatFs.h | USBMSCHFatFs driver interface |
| USBMSCHFatFsTiva.h | USBMSCHFatFs driver implementation for a Tiva USB controller used with the USBMSCHFatFs driver |
| Watchdog.h | Watchdog driver interface |
| WatchdogCC26XX.h | Watchdog driver implementation for CC13XX/CC26XX |
| WatchdogCC3200.h | Watchdog driver implementation for CC3200 |
| WatchdogMSP430.h | Watchdog driver implementation for MSP430 |
| WatchdogMSP432.h | Watchdog driver implementation for MSP432 |
| WatchdogTiva.h | Watchdog driver implementation for Tiva |
| WiFi.h | WiFi driver interface |
| WiFiCC3100.h | WiFi driver implementation for the SimpleLink Wi-Fi CC3100 device |
| WiFiCC3200.h | WiFi driver implementation for the SimpleLink Wi-Fi CC3200 device |