TI-RTOS Drivers  tidrivers_cc13xx_cc26xx_2_20_01_10
Data Fields
NVS_Params Struct Reference

NVS Parameters. More...

#include <NVS.h>

Data Fields

bool eraseOnOpen
 

Detailed Description

NVS Parameters.

NVS parameters are used with the NVS_open() call. Default values for these parameters are set using NVS_Params_init().

See also
NVS_Params_init()

Field Documentation

bool NVS_Params::eraseOnOpen

Erase block on open


The documentation for this struct was generated from the following file:
Copyright 2016, Texas Instruments Incorporated