TI-RTOS Drivers  tidrivers_cc13xx_cc26xx_2_20_01_10
Macros
Collaboration diagram for Status Codes:

Macros

#define USBMSCHFatFs_STATUS_SUCCESS   0
 Successful status code returned by USBMSCHFatFs_control(). More...
 
#define USBMSCHFatFs_STATUS_ERROR   -1
 Generic error status code returned by USBMSCHFatFs_control(). More...
 
#define USBMSCHFatFs_STATUS_UNDEFINEDCMD   -2
 An error status code returned by USBMSCHFatFs_control() for undefined command codes. More...
 

Detailed Description

USBMSCHFatFs_STATUS_* macros are general status codes returned by USBMSCHFatFs_control()

Macro Definition Documentation

#define USBMSCHFatFs_STATUS_SUCCESS   0

Successful status code returned by USBMSCHFatFs_control().

USBMSCHFatFs_control() returns USBMSCHFatFs_STATUS_SUCCESS if the control code was executed successfully.

#define USBMSCHFatFs_STATUS_ERROR   -1

Generic error status code returned by USBMSCHFatFs_control().

USBMSCHFatFs_control() returns USBMSCHFatFs_STATUS_ERROR if the control code was not executed successfully.

#define USBMSCHFatFs_STATUS_UNDEFINEDCMD   -2

An error status code returned by USBMSCHFatFs_control() for undefined command codes.

USBMSCHFatFs_control() returns USBMSCHFatFs_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.

Copyright 2016, Texas Instruments Incorporated