TI-RTOS Drivers
tidrivers_cc13xx_cc26xx_2_20_01_10
|
Macros | |
#define | SDSPI_STATUS_SUCCESS 0 |
Successful status code returned by SDSPI_control(). More... | |
#define | SDSPI_STATUS_ERROR -1 |
Generic error status code returned by SDSPI_control(). More... | |
#define | SDSPI_STATUS_UNDEFINEDCMD -2 |
An error status code returned by SDSPI_control() for undefined command codes. More... | |
SDSPI_STATUS_* macros are general status codes returned by SDSPI_control()
#define SDSPI_STATUS_SUCCESS 0 |
Successful status code returned by SDSPI_control().
SDSPI_control() returns SDSPI_STATUS_SUCCESS if the control code was executed successfully.
#define SDSPI_STATUS_ERROR -1 |
Generic error status code returned by SDSPI_control().
SDSPI_control() returns SDSPI_STATUS_ERROR if the control code was not executed successfully.
#define SDSPI_STATUS_UNDEFINEDCMD -2 |
An error status code returned by SDSPI_control() for undefined command codes.
SDSPI_control() returns SDSPI_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.