TI-RTOS Drivers  tidrivers_cc13xx_cc26xx_2_20_01_10
Data Structures | Macros | Typedefs | Enumerations | Functions
CryptoCC26XX.h File Reference

Detailed Description

Crypto driver implementation for a CC26XX Crypto controller.

============================================================================

Driver Include

The Crypto header file should be included in an application as follows:

Overview

The CryptoCC26XX driver simplifies reading and writing to the CryptoCC26XX peripheral on the board with multiple modes of operation and performance. These include blocking and polling. A timeout can be configured in blocking mode. The driver supports encryption and decryption for both AES-ECB and AES-CCM.

General Behavior

For code examples, see Use Cases below.

Warning
The application should not attempt to encrypt a value stored in flash or use a key stored in flash if the application might switch to the XOSC_HF, the high frequency external oscillator, during the operation.

Opening the driver

// Declaration (typically done in a task)
bool exclusiveAccess = false;
// Initialize Crypto driver
// Configure CryptoCC26XX parameters.
// Attempt to open CryptoCC26XX.
handle = CryptoCC26XX_open(Board_CRYPTO, exclusiveAccess, &params);
if (!handle) {
System_printf("CryptoCC26XX did not open");
}

Before starting a crypto operation

Performing a crypto operation

Supported transaction modes

Closing the driver

The crypto driver is closed by calling CryptoCC26XX_close() function. When the openCnt is decremented to zero, the crypto related bios modules are destructed.

Error handling

If an error occur during encryption/decryption, the operation will return the error code and the device might enter standby.

Power Management

During a transaction in blocking mode, the Power_SB_DISALLOW constraint is set to block the system from entering standby mode. During this period the system will enter idle mode if no tasks are running.

A system dependency on crypto will be active as long as there are clients with an open handle to the crypto.

Note
When coming out of standby the key store RAM has lost it's content, so the keyStore in CryptoCC26XX_Object will be cleared and the clients will have to allocate the key over again.

Supported Functions

API function Description
CryptoCC26XX_init() Function to initializes bios modules needed by CryptoCC26XX module
CryptoCC26XX_open() Initialize Crypto and get crypto handle
CryptoCC26XX_close() Disable Crypto HW and destruct bios modules used by transactions
CryptoCC26XX_Params_init() Initialize Crypto parameters
CryptoCC26XX_Transac_init() Initialize Crypto transaction
CryptoCC26XX_allocateKey() Allocate a key for current client and write key into one of the Crypto RAM locations
CryptoCC26XX_releaseKey() Release/deallocate a key for current client
CryptoCC26XX_transact() Start a crypto operation in blocking mode
CryptoCC26XX_transactPolling() Start a crypto operation in polling mode

Unsupported functionality:

Functionality that currently not supported:

Supported Operations

Operation Type Description
CRYPTOCC26XX_OP_AES_CCM_ENCRYPT AES-CCM encryption of plaintext and authentication of AAD and plaintext
CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY AES-CCM authentication of AAD only. No payload. Encryption of MAC
CRYPTOCC26XX_OP_AES_CCM_DECRYPT AES-CCM decryption of plaintext and authentication of AAD and plaintext
CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY AES-CCM authentication of AAD only. No payload. Encryption of MAC
CRYPTOCC26XX_OP_AES_ECB_ENCRYPT AES-ECB encryption
CRYPTOCC26XX_OP_AES_ECB_DECRYPT AES-ECB decryption
CRYPTOCC26XX_OP_AES_CBC_ENCRYPT AES-CBC encryption
CRYPTOCC26XX_OP_AES_CBC_DECRYPT AES-CBC decryption

Use Cases

AES ECB operation

Perform a crypto operation with AES-ECB in CRYPTOCC26XX_MODE_BLOCKING.

// AES-ECB example struct
typedef struct
{
uint8_t aesKey[16]; // Stores the Aes Key
CryptoCC26XX_KeyLocation aesKeyLocation; // Location in Key RAM
uint8_t aesClearText[16]; // Input message - cleartext
uint8_t aesMsgOut[16]; // Output message
} AESECBExample;
// AES ECB example data
AESECBExample ecbExample =
{
{ 0x2B, 0x7E, 0x15, 0x16, 0x28, 0xAE, 0xD2, 0xA6,
0xAB, 0xF7, 0x15, 0x88, 0x09, 0xCF, 0x4F, 0x3C },
{ 0x6B, 0xC1, 0xBE, 0xE2, 0x2E, 0x40, 0x9F, 0x96,
0xE9, 0x3D, 0x7E, 0x11, 0x73, 0x93, 0x17, 0x2A },
{ 0x3A, 0xD7, 0x7B, 0xB4, 0x0D, 0x7A, 0x36, 0x60,
0xA8, 0x9E, 0xCA, 0xF3, 0x24, 0x66, 0xEF, 0x97 }
};
// Declaration (typically done in a task)
int keyIndex;
// Initialize Crypto driver
// Configure CryptoCC26XX parameters.
// Initialize transaction
// Attempt to open CryptoCC26XX.
handle = CryptoCC26XX_open(Board_CRYPTO, false, &params);
if (!handle) {
System_printf("CryptoCC26XX did not open");
} else {
keyIndex = CryptoCC26XX_allocateKey(handle, ecbExample.aesKeyLocation,
(const uint32_t *) ecbExample.aesKey);
if (keyIndex != CRYPTOCC26XX_STATUS_ERROR) {
// Setup transaction
trans.keyIndex = keyIndex;
trans.msgIn = (uint32_t *) ecbExample.aesClearText;
trans.msgOut = (uint32_t *) ecbExample.aesMsgOut;
// Do AES-ECB operation
CryptoCC26XX_releaseKey(handle, &keyIndex);
} else {
System_printf("Key Location was not allocated.");
}
}

AES CCM operation

Perform a crypto and authentication operation with AES-CCM in CRYPTOCC26XX_MODE_BLOCKING.

#define macLength (4)
#define clearTextLength (16)
#define cipherTextLength (macLength + clearTextLength)
#define nonceLength (12)
#define aadLength (14)
// Holds the AES-CCM setup for this example
typedef struct
{
uint8_t key[16]; // A 128 Bit AES key
CryptoCC26XX_KeyLocation keyLocation; // One of 8 key locations in the hardware
uint8_t clearAndCipherText[cipherTextLength]; // Holds the cleartext before, and the ciphertext
// after the encryption operation.
// Ciphertext = encrypted text + message authentication code (MAC).
uint8_t nonce[nonceLength]; // A value that is used only once (cryptographic term 'nonce')
uint8_t header[aadLength]; // A header that is not encrypted but is authenticated in the operation (AAD).
} AesCcmExample;
AesCcmExample ccmSetup =
{
.key = { 0x2B, 0x7E, 0x15, 0x16, 0x28, 0xAE, 0xD2, 0xA6,
0xAB, 0xF7, 0x15, 0x88, 0x09, 0xCF, 0x4F, 0x3C },
.keyLocation = CRYPTOCC26XX_KEY_0,
.clearAndCipherText = { 't','h','i','s','i','s','a','p','l','a','i','n','t','e','x','t','0','0','0','0' },
.nonce = { 't','h','i','s','i','s','a','n','o','n','c','e' },
.header = { 't','h','i','s','i','s','a','h','e','a','d','e','r','1' }
};
int32_t keyIndex;
int32_t status;
// Initialize Crypto driver structures
// Open the crypto hardware with non-exclusive access and default parameters.
handle = CryptoCC26XX_open(Board_CRYPTO, false, NULL);
if (handle == NULL) {
System_abort("CryptoCC26XX did not open");
}
// Allocate a key storage location in the hardware
keyIndex = CryptoCC26XX_allocateKey(handle, ccmSetup.keyLocation, (const uint32_t *) ccmSetup.key);
if (keyIndex == CRYPTOCC26XX_STATUS_ERROR) {
System_abort("Key Location was not allocated.");
}
// Encrypt and authenticate the message
trans.keyIndex = keyIndex;
trans.authLength = macLength;
trans.nonce = (char *) ccmSetup.nonce;
trans.header = (char *) ccmSetup.header;
trans.fieldLength = 3;
trans.msgInLength = clearTextLength;
trans.headerLength = aadLength;
trans.msgIn = (char *) &(ccmSetup.clearAndCipherText[0]); // Message is encrypted in place
trans.msgOut = (char *) &(ccmSetup.clearAndCipherText[clearTextLength]); // MAC will be written to this position
status = CryptoCC26XX_transact(handle, (CryptoCC26XX_Transaction *) &trans);
System_abort("Encryption and signing failed.");
}
// Decrypt and authenticate message
trans.keyIndex = keyIndex;
trans.authLength = macLength;
trans.nonce = (char *) ccmSetup.nonce;
trans.header = (char *) ccmSetup.header;
trans.fieldLength = 3;
trans.msgInLength = cipherTextLength;
trans.headerLength = aadLength;
trans.msgIn = (char *) &(ccmSetup.clearAndCipherText[0]); // Message is decrypted in place
trans.msgOut = (char *) &(ccmSetup.clearAndCipherText[clearTextLength]); // Points to the MAC, is used as input here
// Do AES-CCM decryption and authentication
status = CryptoCC26XX_transact(handle, (CryptoCC26XX_Transaction *) &trans);
System_abort("Decryption and authentication failed.");
}
// Release the key location
status = CryptoCC26XX_releaseKey(handle, &keyIndex);
System_abort("Key release was not successful.");
}

Instrumentation

The CryptoCC26XX driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 Basic CryptoCC26XX operations performed
Diags_USER2 Detailed CryptoCC26XX operations performed

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/Power.h>
#include <driverlib/crypto.h>
#include <ti/sysbios/family/arm/m3/Hwi.h>
#include <ti/sysbios/knl/Semaphore.h>
Include dependency graph for CryptoCC26XX.h:

Go to the source code of this file.

Data Structures

struct  CryptoCC26XX_Params
 CryptoCC26XX Parameters. More...
 
struct  CryptoCC26XX_Transaction
 CryptoCC26XX Transaction. More...
 
struct  CryptoCC26XX_AESCCM_Transaction
 CryptoCC26XX AES-CCM Transaction. More...
 
struct  CryptoCC26XX_AESCBC_Transaction
 CryptoCC26XX AES-CBC Transaction. More...
 
struct  CryptoCC26XX_AESECB_Transaction
 CryptoCC26XX AES-ECB Transaction. More...
 
struct  CryptoCC26XX_HWAttrs
 CryptoCC26XX Hardware Attributes. More...
 
struct  CryptoCC26XX_Object
 CryptoCC26XX Object. More...
 
struct  CryptoCC26XX_Config
 CryptoCC26XX Global Configuration. More...
 

Macros

#define CRYPTOCC26XX_TIMEOUT   20
 
#define CRYPTOCC26XX_STATUS_SUCCESS   0
 
#define CRYPTOCC26XX_STATUS_ERROR   -1
 
#define CRYPTOCC26XX_STATUS_UNDEFINEDCMD   -2
 
#define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT   0
 
#define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY   1
 
#define CRYPTOCC26XX_OP_AES_CCM_DECRYPT   2
 
#define CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY   3
 
#define CRYPTOCC26XX_OP_AES_ECB_ENCRYPT   4
 
#define CRYPTOCC26XX_OP_AES_ECB_DECRYPT   5
 
#define CRYPTOCC26XX_OP_AES_CBC_ENCRYPT   6
 
#define CRYPTOCC26XX_OP_AES_CBC_DECRYPT   7
 
#define CRYPTOCC26XX_OP_AES_CCM   CRYPTOCC26XX_OP_AES_CCM_ENCRYPT
 
#define CRYPTOCC26XX_OP_AES_CCM_NOCRYPT   CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY
 
#define CRYPTOCC26XX_OP_AES_CCMINV   CRYPTOCC26XX_OP_AES_CCM_DECRYPT
 
#define CRYPTOCC26XX_OP_AES_CCMINV_NOCRYPT   CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY
 
#define CRYPTOCC26XX_OP_AES_ECB   CRYPTOCC26XX_OP_AES_ECB_ENCRYPT
 
#define CRYPTOCC26XX_OP_AES_ECB_NOCRYPT   CRYPTOCC26XX_OP_AES_ECB_DECRYPT
 
#define ti_sysbios_family_arm_m3_Hwi__nolocalnames
 

Typedefs

typedef struct CryptoCC26XX_ConfigCryptoCC26XX_Handle
 A handle that is returned from a CryptoCC26XX_open() call. More...
 
typedef enum CryptoCC26XX_Mode CryptoCC26XX_Mode
 CryptoCC26XX Mode Settings. More...
 
typedef uint8_t CryptoCC26XX_Operation
 CryptoCC26XX Operation Type. More...
 
typedef enum CryptoCC26XX_KeyLocation CryptoCC26XX_KeyLocation
 CryptoCC26XX Key Store Location. More...
 
typedef struct CryptoCC26XX_Params CryptoCC26XX_Params
 CryptoCC26XX Parameters. More...
 
typedef uint8_t CryptoCC26XX_KeyStore
 CryptoCC26XX Key. More...
 
typedef struct CryptoCC26XX_Transaction CryptoCC26XX_Transaction
 CryptoCC26XX Transaction. More...
 
typedef struct CryptoCC26XX_AESCCM_Transaction CryptoCC26XX_AESCCM_Transaction
 CryptoCC26XX AES-CCM Transaction. More...
 
typedef struct CryptoCC26XX_AESCBC_Transaction CryptoCC26XX_AESCBC_Transaction
 CryptoCC26XX AES-CBC Transaction. More...
 
typedef struct CryptoCC26XX_AESECB_Transaction CryptoCC26XX_AESECB_Transaction
 CryptoCC26XX AES-ECB Transaction. More...
 
typedef struct CryptoCC26XX_HWAttrs CryptoCC26XX_HWAttrs
 CryptoCC26XX Hardware Attributes. More...
 
typedef struct CryptoCC26XX_Object CryptoCC26XX_Object
 CryptoCC26XX Object. More...
 
typedef struct CryptoCC26XX_Config CryptoCC26XX_Config
 CryptoCC26XX Global Configuration. More...
 

Enumerations

enum  CryptoCC26XX_Mode {
  CRYPTOCC26XX_MODE_BLOCKING,
  CRYPTOCC26XX_MODE_POLLING
}
 CryptoCC26XX Mode Settings. More...
 
enum  CryptoCC26XX_KeyLocation {
  CRYPTOCC26XX_KEY_0 = 0,
  CRYPTOCC26XX_KEY_1,
  CRYPTOCC26XX_KEY_2,
  CRYPTOCC26XX_KEY_3,
  CRYPTOCC26XX_KEY_4,
  CRYPTOCC26XX_KEY_5,
  CRYPTOCC26XX_KEY_6,
  CRYPTOCC26XX_KEY_7,
  CRYPTOCC26XX_KEY_COUNT,
  CRYPTOCC26XX_KEY_ANY
}
 CryptoCC26XX Key Store Location. More...
 

Functions

int CryptoCC26XX_close (CryptoCC26XX_Handle handle)
 Function to closes a given CryptoCC26XX peripheral specified by the CryptoCC26XX handle. More...
 
void CryptoCC26XX_init (void)
 Function to initializes bios modules needed by CryptoCC26XX module. More...
 
CryptoCC26XX_Handle CryptoCC26XX_open (unsigned int index, bool exclusiveAccess, CryptoCC26XX_Params *params)
 Function to initialize a given CryptoCC26XX peripheral specified by the particular index value. The parameter specifies which mode the CryptoCC26XX will operate. More...
 
void CryptoCC26XX_Params_init (CryptoCC26XX_Params *params)
 Function to initialize the CryptoCC26XX_Params struct to its defaults. More...
 
void CryptoCC26XX_Transac_init (CryptoCC26XX_Transaction *trans, CryptoCC26XX_Operation opType)
 Function to initialize the CryptoCC26XX_Transaction struct to its defaults. More...
 
int CryptoCC26XX_allocateKey (CryptoCC26XX_Handle handle, CryptoCC26XX_KeyLocation keyLocation, const uint32_t *keySrc)
 Function that allocates key, writes key into key store RAM and returns a handle to CryptoCC26XX Key. More...
 
int CryptoCC26XX_loadKey (CryptoCC26XX_Handle handle, int keyIndex, const uint32_t *keySrc)
 Function that writes a given key into a key store. More...
 
int CryptoCC26XX_releaseKey (CryptoCC26XX_Handle handle, int *keyIndex)
 Function that releases the specified CryptoCC26XX Key. More...
 
int CryptoCC26XX_transact (CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
 Function to do a Crypto operation (encryption or decryption) in blocking mode. More...
 
int CryptoCC26XX_transactPolling (CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
 Function to do a Crypto transaction operation (encryption or decryption) in polling mode. More...
 
int CryptoCC26XX_transactCallback (CryptoCC26XX_Handle handle, CryptoCC26XX_Transaction *transaction)
 Function to do a Crypto transaction operation (encryption or decryption) in callback mode. Currently not supported. More...
 

Macro Definition Documentation

#define CRYPTOCC26XX_TIMEOUT   20

Timeout Return Code

#define CRYPTOCC26XX_STATUS_SUCCESS   0

Success Return Code

#define CRYPTOCC26XX_STATUS_ERROR   -1

Error Return Code

#define CRYPTOCC26XX_STATUS_UNDEFINEDCMD   -2

Command Undefined Return Code

#define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT   0

AES-CCM encryption of both AAD and plain text

#define CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY   1

AES-CCM authentication of ADD only

#define CRYPTOCC26XX_OP_AES_CCM_DECRYPT   2

AES-CCM decryption of both AAD and plain text

#define CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY   3

AES-CCM authentication of ADD only

#define CRYPTOCC26XX_OP_AES_ECB_ENCRYPT   4

AES-ECB encryption

#define CRYPTOCC26XX_OP_AES_ECB_DECRYPT   5

AES-ECB decryption

#define CRYPTOCC26XX_OP_AES_CBC_ENCRYPT   6

AES-CBC encryption

#define CRYPTOCC26XX_OP_AES_CBC_DECRYPT   7

AES-CBC decryption

#define CRYPTOCC26XX_OP_AES_CCM   CRYPTOCC26XX_OP_AES_CCM_ENCRYPT
#define CRYPTOCC26XX_OP_AES_CCM_NOCRYPT   CRYPTOCC26XX_OP_AES_CCM_ENCRYPT_AAD_ONLY
#define CRYPTOCC26XX_OP_AES_CCMINV   CRYPTOCC26XX_OP_AES_CCM_DECRYPT
#define CRYPTOCC26XX_OP_AES_CCMINV_NOCRYPT   CRYPTOCC26XX_OP_AES_CCM_DECRYPT_AAD_ONLY
#define CRYPTOCC26XX_OP_AES_ECB   CRYPTOCC26XX_OP_AES_ECB_ENCRYPT
#define CRYPTOCC26XX_OP_AES_ECB_NOCRYPT   CRYPTOCC26XX_OP_AES_ECB_DECRYPT
#define ti_sysbios_family_arm_m3_Hwi__nolocalnames

Typedef Documentation

A handle that is returned from a CryptoCC26XX_open() call.

CryptoCC26XX Mode Settings.

This enum defines the read and write modes for the configured CryptoCC26XX.

typedef uint8_t CryptoCC26XX_Operation

CryptoCC26XX Key Store Location.

This enumeration defines the possible key locations in CryptoCC26XX.

CryptoCC26XX Parameters.

typedef uint8_t CryptoCC26XX_KeyStore

CryptoCC26XX Key.

This holds allocation information for the keys in the key store.

CryptoCC26XX Transaction.

This structure defines the nature of a general crypto transaction. An operation specific object, e.g. CryptoCC26XX_AESCCM_Transaction, must be used by the clients. All transaction must be typecasted to this common type when calling the transact functions. The first data of all transactions must hold a type field indicating which type of transaction to be performed.

CryptoCC26XX AES-CCM Transaction.

The Counter with CBC-MAC (CCM) mode of operation is a generic authenticated encryption block cipher mode. It can be used with any 128-bit block cipher. AES-CCM combines CBC-MAC with an AES block cipher.

AES-CCM encryption has the following inputs and outputs:

AES-CCM input and output parameters
EncryptionDecryption
Input
Shared AES keyShared AES key
NonceNonce
CleartextCiphertext (encrypted cleartext + MAC)
AAD (optional)AAD (optional)
Output
Ciphertext (encrypted cleartext + MAC)Cleartext

The AES key is a shared secret between the two parties and has a length of 128 Bit. The key is stored in the dedicated RAM of the AES hardware unit before the crypto operation.

The nonce is generated by the party performing the authenticated encryption operation. Within the scope of any authenticated encryption key, the nonce value must be unique. That is, the set of nonce values used with any given key must not contain any duplicate values. Using the same nonce for two different messages encrypted with the same key destroys the security properties.

The optional AAD is authenticated, but not encrypted. Thus, the AAD is not included in the AES-CCM output. It can be used to authenticate packet headers for transport layer security.

After the encryption operation, the ciphertext contains the encrypted data and the message authentication code (MAC). The MAC can be seen as an encrypted fingerprint of the message header and content.

AES-CCM works in both ways: encryption and decryption. When a message is decrypted, then ciphertext, AAD and nonce are used as inputs while the output comprises the cleartext only. The decryption operation is successful, when the received ciphertext, the nonce and the AAD can reproduce the containing MAC.

The CryptoCC26XX_AESCCM_Transaction structure defines all necessary parameters for a AES-CCM transaction.

CryptoCC26XX AES-CBC Transaction.

This structure defines the nature of the AES-CBC transaction. An object of this structure must be initialized by calling CryptoCC26XX_Transac_init().

CryptoCC26XX AES-ECB Transaction.

This structure defines the nature of the AES-ECB transaction. An object of this structure must be initialized by calling CryptoCC26XX_Transac_init().

CryptoCC26XX Hardware Attributes.

These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC26XXWare these definitions are found in:

  • inc/hw_memmap.h
  • inc/hw_ints.h

intPriority is the Crypto peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.drivers.ports interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().

A sample structure is shown below:

1 const CryptoCC26XX_HWAttrs cryptoCC26XXHWAttrs[] = {
2  {
3  .baseAddr = CRYPTO_BASE,
4  .powerMngrId = PERIPH_CRYPTO,
5  .intNum = INT_CRYPTO,
6  .intPriority = (~0)
7  }
8 };

CryptoCC26XX Object.

The application must not access any member variables of this structure!

CryptoCC26XX Global Configuration.

Enumeration Type Documentation

CryptoCC26XX Mode Settings.

This enum defines the read and write modes for the configured CryptoCC26XX.

Enumerator
CRYPTOCC26XX_MODE_BLOCKING 

Uses a semaphore to block while data is being sent. Context of the call must be a Task.

CRYPTOCC26XX_MODE_POLLING 

Will return when the operation has finished. Call can be made from hwi and swi context.

CryptoCC26XX Key Store Location.

This enumeration defines the possible key locations in CryptoCC26XX.

Enumerator
CRYPTOCC26XX_KEY_0 
CRYPTOCC26XX_KEY_1 
CRYPTOCC26XX_KEY_2 
CRYPTOCC26XX_KEY_3 
CRYPTOCC26XX_KEY_4 
CRYPTOCC26XX_KEY_5 
CRYPTOCC26XX_KEY_6 
CRYPTOCC26XX_KEY_7 
CRYPTOCC26XX_KEY_COUNT 
CRYPTOCC26XX_KEY_ANY 

Function Documentation

int CryptoCC26XX_close ( CryptoCC26XX_Handle  handle)

Function to closes a given CryptoCC26XX peripheral specified by the CryptoCC26XX handle.

Precondition
CryptoCC26XX_open() had to be called first. Calling context: Task
Parameters
handleA CryptoCC26XX_Handle returned from CryptoCC26XX_open().
Returns
Returns CRYPTOCC26XX_STATUS_SUCCESS if successful, otherwise will return CRYPTOCC26XX_STATUS_ERROR.
See also
CryptoCC26XX_open
void CryptoCC26XX_init ( void  )

Function to initializes bios modules needed by CryptoCC26XX module.

Precondition
This function must be called before any other CryptoCC26XX driver APIs. Calling context: Task and Main.
CryptoCC26XX_Handle CryptoCC26XX_open ( unsigned int  index,
bool  exclusiveAccess,
CryptoCC26XX_Params params 
)

Function to initialize a given CryptoCC26XX peripheral specified by the particular index value. The parameter specifies which mode the CryptoCC26XX will operate.

Precondition
The CryptoCC26XX_Config structure must exist and be persistent before this function can be called. CryptoCC26XX has been initialized with CryptoCC26XX_init(). Calling context: Task.
Parameters
indexLogical peripheral number indexed into the HWAttrs table.
exclusiveAccessBoolean flag to get exclusive access, if true all subsequent calls to CryptoCC26XX_open() will fail.
paramsPointer to an parameter block, if NULL it will use default values.
Returns
A CryptoCC26XX_Handle on success or a NULL on an error or if it has been already opened with exclusiveAccess set.
See also
CryptoCC26XX_close(), CryptoCC26XX_init()
void CryptoCC26XX_Params_init ( CryptoCC26XX_Params params)

Function to initialize the CryptoCC26XX_Params struct to its defaults.

Precondition
Calling context: Hwi, Swi and Task.

Defaults values are: timeout = BIOS_WAIT_FOREVER;

Parameters
paramsParameter structure to initialize.
void CryptoCC26XX_Transac_init ( CryptoCC26XX_Transaction trans,
CryptoCC26XX_Operation  opType 
)

Function to initialize the CryptoCC26XX_Transaction struct to its defaults.

Precondition
Calling context: Hwi, Swi and Task.
Parameters
transTransaction structure to initialize.
opTypeCryto Operation type to perform in the transaction. See CryptoCC26XX_Operation for currently supported types.
int CryptoCC26XX_allocateKey ( CryptoCC26XX_Handle  handle,
CryptoCC26XX_KeyLocation  keyLocation,
const uint32_t *  keySrc 
)

Function that allocates key, writes key into key store RAM and returns a handle to CryptoCC26XX Key.

This function tries to allocate the wanted key location, initiates an operation to write a key into one of the keystore RAM entries and returns a key index integer to the calling client. The allocated key index shall be used when building a transaction data object, e.g. CryptoCC26XX_AESCCM_Transaction.keyIndex. The function blocks the task calling it until the crypto hardware is available.

Precondition
CryptoCC26XX_open() has to be called first. Calling context: Hwi, Swi and Task.
Parameters
handleA CryptoCC26XX_Handle returned by CryptoCC26XX_open().
keyLocationThe key location in key store to allocate. If set to CRYPTOCC26XX_KEY_ANY, the first available key, starting from highest index, will be allocated.
keySrcA pointer to buffer containing key to be written. If this pointer is NULL, the key store will be reserved for the handle, but no key will be written to the key store.
Returns
An integer representing the index allocated in key store or a CRYPTOCC26XX_STATUS_ERROR on an error.
See also
CryptoCC26XX_releaseKey()
CryptoCC26XX_loadKey()
int CryptoCC26XX_loadKey ( CryptoCC26XX_Handle  handle,
int  keyIndex,
const uint32_t *  keySrc 
)

Function that writes a given key into a key store.

This function loads a key into a keystore without needing to release the key store and re-allocate it using CryptoCC26XX_releaseKey() and CryptoCC26XX_allocateKey(). The function blocks the task calling it until the crypto hardware is available.

Precondition
CryptoCC26XX_open() and CryptoCC26XX_allocateKey() have to be called first. Calling context: Hwi, Swi and Task.
Parameters
handleA CryptoCC26XX_Handle returned by CryptoCC26XX_open().
keyIndexA key index returned by a previous call to CryptoCC26XX_allocateKey().
keySrcA pointer to buffer containing a key.
Returns
An integer representing success (CRYPTOCC26XX_STATUS_SUCCESS) or an error (CRYPTOCC26XX_STATUS_ERROR).
See also
CryptoCC26XX_releaseKey()
CryptoCC26XX_loadKey()
int CryptoCC26XX_releaseKey ( CryptoCC26XX_Handle  handle,
int *  keyIndex 
)

Function that releases the specified CryptoCC26XX Key.

This function releases the crypto key, so it can be used by other clients.

Precondition
Driver must have been opened and the key must have been allocated first. Calling context: Hwi, Swi and Task.
Parameters
handleA CryptoCC26XX_Handle returned by CryptoCC26XX_open().
keyIndexA pointer to the keyIndex to be released.
Returns
Returns CRYPTOCC26XX_STATUS_SUCCESS if successful, otherwise will return CRYPTOCC26XX_STATUS_ERROR.
See also
CryptoCC26XX_allocateKey()
int CryptoCC26XX_transact ( CryptoCC26XX_Handle  handle,
CryptoCC26XX_Transaction transaction 
)

Function to do a Crypto operation (encryption or decryption) in blocking mode.

This function initiates a blocking crypto operation.

CryptoCC26XX_transact() will block task execution until all the data has been encrypted or decrypted, a task switch could be done when pending on a semaphore.

Precondition
Driver must have been opened and a key must have been allocated first. Calling context: Task.
Parameters
handleA CryptoCC26XX_Handle returned by CryptoCC26XX_open().
transactionPointer to a transaction descriptor.
Returns
Returns CRYPTOCC26XX_STATUS_SUCCESS if successful, error code if not.
See also
CryptoCC26XX_open(), CryptoCC26XX_allocateKey(), CryptoCC26XX_transactPolling()
int CryptoCC26XX_transactPolling ( CryptoCC26XX_Handle  handle,
CryptoCC26XX_Transaction transaction 
)

Function to do a Crypto transaction operation (encryption or decryption) in polling mode.

This function initiates a polling crypto operation.

CryptoCC26XX_transactPolling() blocks task execution and does not pend on a semaphore, consequently no task switch will be done as a result of pending.

Precondition
Driver must have been opened and a key must have been allocated first. Calling context: Hwi, Swi and Task.
Parameters
handleAn CryptoCC26XX_Handle returned by CryptoCC26XX_open().
transactionPointer to a transaction descriptor.
Returns
Returns CRYPTOCC26XX_STATUS_SUCCESS if successful, error code if not.
See also
CryptoCC26XX_open(), CryptoCC26XX_allocateKey(), CryptoCC26XX_transact()
int CryptoCC26XX_transactCallback ( CryptoCC26XX_Handle  handle,
CryptoCC26XX_Transaction transaction 
)

Function to do a Crypto transaction operation (encryption or decryption) in callback mode. Currently not supported.

This function initiates a callback crypto operation.

CryptoCC26XX_transactCallback() will continue task execution (i.e. does not pend on a semaphore). A callback function must be defined, and will be called when the crypto operation has finished.

Precondition
Driver must have been opened and a key must have been allocated first. Calling context: Hwi, Swi and Task.
Parameters
handleAn CryptoCC26XX_Handle returned by CryptoCC26XX_open().
transactionPointer to a transaction descriptor.
Returns
Returns CRYPTOCC26XX_STATUS_SUCCESS if successful, error code if not.
Note
Currently not supported. Will replace CryptoCC26XX_transactPolling in the future.
See also
CryptoCC26XX_open(), CryptoCC26XX_allocateKey(), CryptoCC26XX_transact()
Copyright 2016, Texas Instruments Incorporated