63 #ifndef ti_driver_pwm_PWMTimerTiva__include
64 #define ti_driver_pwm_PWMTimerTiva__include
uint8_t gpioPinIndex
Definition: PWMTimerTiva.h:138
PWM_Duty_Units
PWM duty cycle unit definitions. Refer to device specific implementation if using PWM_DUTY_COUNTS (ra...
Definition: PWM.h:237
PWMTimerTiva Object.
Definition: PWMTimerTiva.h:146
uint32_t period
Definition: PWMTimerTiva.h:148
struct PWMTimerTiva_HWAttrsV1 PWMTimerTiva_HWAttrsV1
PWMTimerTiva Hardware attributes.
uint32_t gpioBaseAddr
Definition: PWMTimerTiva.h:136
PWM_Period_Units
PWM period unit definitions. Refer to device specific implementation if using PWM_PERIOD_COUNTS (raw ...
Definition: PWM.h:227
bool isOpen
Definition: PWMTimerTiva.h:152
PWM_IdleLevel idleLevel
Definition: PWMTimerTiva.h:151
uint16_t halfTimer
Definition: PWMTimerTiva.h:131
PWM_Duty_Units dutyUnits
Definition: PWMTimerTiva.h:149
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:331
PWMTimerTiva Hardware attributes.
Definition: PWMTimerTiva.h:127
uint32_t timerBaseAddr
Definition: PWMTimerTiva.h:129
uint32_t duty
Definition: PWMTimerTiva.h:147
PWM_IdleLevel
Idle output level when PWM is not running (stopped / not started).
Definition: PWM.h:246
uint32_t pinTimerPwmMode
Definition: PWMTimerTiva.h:133
struct PWMTimerTiva_Object PWMTimerTiva_Object
PWMTimerTiva Object.
PWM_Period_Units periodUnits
Definition: PWMTimerTiva.h:150
const PWM_FxnTable PWMTimerTiva_fxnTable