![]() |
![]() |
TI-RTOS Drivers
tidrivers_cc32xx_2_16_00_08
|
![]() |
Macros | |
#define | USBMSCHFatFs_STATUS_SUCCESS 0 |
Successful status code returned by USBMSCHFatFs_control(). More... | |
#define | USBMSCHFatFs_STATUS_ERROR -1 |
Generic error status code returned by USBMSCHFatFs_control(). More... | |
#define | USBMSCHFatFs_STATUS_UNDEFINEDCMD -2 |
An error status code returned by USBMSCHFatFs_control() for undefined command codes. More... | |
USBMSCHFatFs_STATUS_* macros are general status codes returned by USBMSCHFatFs_control()
#define USBMSCHFatFs_STATUS_SUCCESS 0 |
Successful status code returned by USBMSCHFatFs_control().
USBMSCHFatFs_control() returns USBMSCHFatFs_STATUS_SUCCESS if the control code was executed successfully.
#define USBMSCHFatFs_STATUS_ERROR -1 |
Generic error status code returned by USBMSCHFatFs_control().
USBMSCHFatFs_control() returns USBMSCHFatFs_STATUS_ERROR if the control code was not executed successfully.
#define USBMSCHFatFs_STATUS_UNDEFINEDCMD -2 |
An error status code returned by USBMSCHFatFs_control() for undefined command codes.
USBMSCHFatFs_control() returns USBMSCHFatFs_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.