![]() |
![]() |
TI-RTOS Drivers
tidrivers_cc32xx_2_16_00_08
|
![]() |
Macros | |
#define | EMAC_STATUS_SUCCESS 0 |
Successful status code returned by EMAC_control(). More... | |
#define | EMAC_STATUS_ERROR -1 |
Generic error status code returned by EMAC_control(). More... | |
#define | EMAC_STATUS_UNDEFINEDCMD -2 |
An error status code returned by EMAC_control() for undefined command codes. More... | |
EMAC_STATUS_* macros are general status codes returned by EMAC_control()
#define EMAC_STATUS_SUCCESS 0 |
Successful status code returned by EMAC_control().
EMAC_control() returns EMAC_STATUS_SUCCESS if the control code was executed successfully.
#define EMAC_STATUS_ERROR -1 |
Generic error status code returned by EMAC_control().
EMAC_control() returns EMAC_STATUS_ERROR if the control code was not executed successfully.
#define EMAC_STATUS_UNDEFINEDCMD -2 |
An error status code returned by EMAC_control() for undefined command codes.
EMAC_control() returns EMAC_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.