Functions | |
void | Route6Msg (uint Msg) |
HANDLE | Rt6Create (UINT32 flags, IP6N IPAddr, IP6N IPMask, IP6N NextHop, UINT8 *mac_address, NETIF_DEVICE *ptr_device, UINT32 ValidLifetime) |
HANDLE | Rt6Modify (HANDLE hRoute6, UINT32 flags, IP6N IPAddr, IP6N IPMask, IP6N NextHop, UINT8 *mac_address, NETIF_DEVICE *ptr_device, UINT32 ValidLifetime) |
void | Rt6Free (HANDLE hRoute6) |
void | Rt6FlushInterfaceRoutes (NETIF_DEVICE *ptr_device) |
HANDLE | Rt6Find (UINT32 Flags, IP6N IPAddress, NETIF_DEVICE *ptr_device) |
HANDLE | Rt6GetLLI (HANDLE hRoute6) |
HANDLE | Rt6GetIF (HANDLE hRoute6) |
UINT32 | Rt6GetMTU (HANDLE hRoute6) |
int | Rt6IsLocalRoute (HANDLE hRoute) |
void | Rt6IncRefCount (HANDLE hRoute6) |
int | Rt6IsDefaultRoute (HANDLE hRoute6) |
void | Rt6GetNetworkAddr (HANDLE hRoute6, IP6N *IPNet) |
HANDLE | Rt6FindDefaultRouter (IP6N RouterAddress, NETIF_DEVICE *ptr_device) |
void | Rt6Update (HANDLE hRoute, UINT32 RxPacketType, UINT8 *mac_address, UINT32 Flags, UINT32 Lifetime) |
RT6_ENTRY * | Rt6GetTable (void) |
void | Rt6CleanTable (RT6_ENTRY *ptr_list) |
void Route6Msg | ( | uint | Msg | ) |
Description
Sevices intialization and resource messages for the ROUTE6 Module
This is for *internal* NDK Stack Usage.
[in] | Msg | The message event which needs to be handled. |
Not | Applicable. |
void Rt6CleanTable | ( | RT6_ENTRY * | ptr_list | ) |
Description
The function is called to clean the memory allocated by a previous call to Route6GetTable. The function cleans the replicated copy of the routing table. This function is available to system developers and can be called from outside kernel mode.
[in] | ptr_list | This is the head of the duplicate list which will be cleaned up. |
Not | Applicable |
HANDLE Rt6Create | ( | UINT32 | flags, | |
IP6N | IPAddr, | |||
IP6N | IPMask, | |||
IP6N | NextHop, | |||
UINT8 * | mac_address, | |||
NETIF_DEVICE * | ptr_device, | |||
UINT32 | ValidLifetime | |||
) |
Description
The function creates a new routing entry.
[in] | flags | Specifies flags. |
[in] | IPAddr | This is the IPv6 address for which the route is created. |
[in] | IPMask | This is the IPv6 subnet mask. |
[in] | NextHop | This is the Next Hop gateway associated with the route. |
[in] | mac_address | This is the MAC Address associated with the ROUTE. This can be NULL. |
[in] | ptr_device | This is the interface on which the route is created. |
[in] | ValidLifetime | Timeout for which this route will remain valid. This is VALID only for CLONING Routes. Once the CLONING Route is timed out all HOST routes derived from this will also be removed. If this is INFINITE_LT then the routes are always active. |
Success | - Handle to the new route | |
Error | - 0 |
HANDLE Rt6Find | ( | UINT32 | Flags, | |
IP6N | IPAddress, | |||
NETIF_DEVICE * | ptr_device | |||
) |
Description
The function searches the routing table for a route to be used.
[in] | Flags | Flags associated with the routing entry. Specifies the SEARCH Parameters that can be used to find a ROUTING Entry. FLG_RTE_HOST -> Search ROUTE6 table for only HOST routes FLG_RTE_CLONING -> Search ROUTE6 table for only NETWORK routes 0 -> Search all ROUTES (Host & Network) but Network routes are not cloned. FLG_RTF_CLONE -> Invalid. FLG_RTE_GATEWAY -> Invalid. (Use the Rt6FindDefaultRouter API) |
[in] | IPAddress | The IPv6 address for which we are trying to find a ROUTE. |
[in] | ptr_device | Device on which the route exists. This can be NULL. |
Match | - Handle to the routing 6 entry | |
No | Match - 0 |
HANDLE Rt6FindDefaultRouter | ( | IP6N | RouterAddress, | |
NETIF_DEVICE * | ptr_device | |||
) |
Description
The function checks if the Router Address Matches an entry in the default Router List.
[in] | RouterAddress | The Default router address we are trying to find. |
[in] | ptr_device | Device on which the default router is being searched. If specified as NULL; then the device is wildcarded and all default routes are searched. |
Match | - Handle to the Default Router | |
No | Match - 0 |
void Rt6FlushInterfaceRoutes | ( | NETIF_DEVICE * | ptr_device | ) |
Description
The function cleans all routes on a specific interface
[in] | ptr_device | Pointer to the device for which all routes will be cleaned. |
Not | Applicable. |
void Rt6Free | ( | HANDLE | hRoute6 | ) |
Description
The function frees an existing routing entry.
[in] | hRoute6 | Route to be deleted. |
Not | Applicable. |
HANDLE Rt6GetIF | ( | HANDLE | hRoute6 | ) |
Description
The function gets the Interface handle associated with the Route6 object.
[in] | hRoute6 | The handle to the route6 object whose Interface handle we are interested in. |
Success | - Handle to the Interface | |
Error | - 0 |
HANDLE Rt6GetLLI | ( | HANDLE | hRoute6 | ) |
Description
The function returns the LLIv6 entry given the Route6 handle
[in] | hRoute6 | The handle to the route6 object whose LLIv6 handle we are interested in. |
Success | - Handle to the LLIv6 | |
Error | - 0 |
UINT32 Rt6GetMTU | ( | HANDLE | hRoute6 | ) |
Description
The function gets the MTU associated with the Route6 object.
[in] | hRoute6 | The handle to the ROUTE6 Object whose MTU we are interested in. |
Success | - MTU of the route. | |
Error | - 0 |
void Rt6GetNetworkAddr | ( | HANDLE | hRoute6, | |
IP6N * | IPNet | |||
) |
Description
The function returns the Network Address associated with a route.
[in] | hRoute6 | The handle to the ROUTE6 Object. |
[out] | IPNet | The handle to the Network Address to be returned. |
None |
RT6_ENTRY* Rt6GetTable | ( | void | ) |
Description
The function replicates the IPv6 Routing Table and creates a duplicate copy which is then returned back to the callee. The replicated routing table list needs to be cleaned by the callee. This function is available to system developers and can be called from outside kernel mode.
Head | of the copy of the IPv6 Routing Table |
void Rt6IncRefCount | ( | HANDLE | hRoute6 | ) |
Description
The function increments the reference count for a route6.
[in] | hRoute6 | The handle to the route6 object whose reference counter needs to be incremented. |
Success | - Handle to the Interface | |
Error | - 0 |
int Rt6IsDefaultRoute | ( | HANDLE | hRoute6 | ) |
Description
The function checks if the route specified is a default route?
[in] | hRoute6 | The handle to the ROUTE6 Object. |
Success | - 1. | |
Error | - 0 |
int Rt6IsLocalRoute | ( | HANDLE | hRoute | ) |
Description
The function checks if the route specified is LOCAL or not?
[in] | hRoute | The handle to the ROUTE6 Object. |
Success | - MTU of the route. | |
Error | - 0 |
HANDLE Rt6Modify | ( | HANDLE | hRoute6, | |
UINT32 | flags, | |||
IP6N | IPAddr, | |||
IP6N | IPMask, | |||
IP6N | NextHop, | |||
UINT8 * | mac_address, | |||
NETIF_DEVICE * | ptr_device, | |||
UINT32 | ValidLifetime | |||
) |
Description
The function modifies an existing routing entry.
[in] | hRoute6 | Handle to the route which is to be modified. |
[in] | flags | Specifies flags. |
[in] | IPAddr | This is the IPv6 address for which the route is created. |
[in] | IPMask | This is the IPv6 subnet mask. |
[in] | NextHop | This is the Next Hop gateway associated with the route. |
[in] | mac_address | This is the MAC Address associated with the ROUTE. This can be NULL. |
[in] | ptr_device | This is the interface on which the route is created. |
[in] | ValidLifetime | Timeout for which this route will remain valid. This is VALID only for CLONING Routes. Once the CLONING Route is timed out all HOST routes derived from this will also be removed. If this is INFINITE_LT then the routes are always active. |
Success | - Handle to the modified route | |
Error | - 0 |
void Rt6Update | ( | HANDLE | hRoute, | |
UINT32 | RxPacketType, | |||
UINT8 * | mac_address, | |||
UINT32 | Flags, | |||
UINT32 | Lifetime | |||
) |
Description
The function is used to update the ROUTE6 and corresponding LLI6 Entry. This is called whenever a Neighbor Discovery Packet is received and the Target Address is meant for us.
[in] | hRoute | Handle to the route we need to update. |
[in] | RxPacketType | Type of NDISC Packet received. |
[in] | mac_address | MAC Address information if present from the NDISC Packet. |
[in] | Flags | The flags field in the Received NA Header. Its set to 0 for all other packets. |
[in] | Lifetime | New Lifetime value to be updated with valid only for RA. Else ignored in this function. |
Not | Applicable |