#include <route6if.h>
Data Fields | |
LIST_NODE | links |
Links to the the next entry. | |
UINT32 | Flags |
Routing Flag Entries. This can be set to Host, Network or Gateway Routes. | |
UINT32 | RefCount |
Reference Counter. | |
UINT32 | dwTimeout |
Expiration time in SECONDS. | |
IP6N | NetworkAddr |
Network Address. | |
IP6N | IPAddr |
IP Address. | |
IP6N | IPMask |
IP Mask. | |
IP6N | NextHop |
Next Hop IP Address. | |
UINT32 | ProtMTU |
Protocol MTU for this route. | |
NETIF_DEVICE * | ptr_device |
Pointer to the network interface on which the route resides. | |
HANDLE | hLLI6 |
HANDLE to the LLI6 Entry. |
There exists an entry for each of the following:-
Thus currently the Flags supported here are:-