Functions | |
void | LLI6Update (HANDLE hLLI6, UINT8 *mac_address, UINT32 RxPktType, UINT32 Flags) |
void | LLI6Msg (uint Msg) |
void | LLI6IncRefCount (HANDLE hLLI6) |
UINT8 | LLI6IsRouter (HANDLE hLLI6) |
UINT8 | LLI6IsDead (HANDLE hLLI6) |
UINT8 | LLI6IsValid (HANDLE hLLI6) |
void | LLI6SetIncomplete (HANDLE hLLI6) |
NETIF_DEVICE * | LLI6GetNetDevice (HANDLE hLLI6) |
HANDLE | LLI6New (RT6_ENTRY *ptr_rt6, UINT8 *pMacAddress, UINT8 IsRouter) |
void | LLI6Free (HANDLE hLLI6) |
void | LLI6TxIPPacket (PBM_Pkt *pPkt, HANDLE hLLI6, NETIF_DEVICE *ptr_device, IP6N Address) |
void LLI6Free | ( | HANDLE | hLLI6 | ) |
Description
This function is used to delete the LLI6 Entry. LLI6 Entries can only be deleted by the ROUTE6 Module.
This is for *internal* NDK Stack Usage.
[in] | hLLI6 | Handle to the LLI6 Object to be deleted. |
Not | Applicable. |
NETIF_DEVICE* LLI6GetNetDevice | ( | HANDLE | hLLI6 | ) |
Description
The function gets the network device associated with the LLI6 Entry.
This is for *internal* NDK Stack Usage.
[in] | hLLI6 | Handle to the LLI6 Entry whose network device we need to return. |
Success | - Handle to the Network Device Error - 0 |
void LLI6IncRefCount | ( | HANDLE | hLLI6 | ) |
Description
The function Increments the reference counter for the LLI6 Entry. This can be invoked by the ROUTE6 Module if it detects multiple hosts which have different IP addresses but are actual one and the same.
This is for *internal* NDK Stack Usage.
[in] | hLLI6 | Handle of the LLI6 Entry whose reference counter we need to increment. |
Not | Applicable. |
UINT8 LLI6IsDead | ( | HANDLE | hLLI6 | ) |
Description
The function checks if the LLI6 Entry is DEAD or not?
This is for *internal* NDK Stack Usage.
[in] | hLLI6 | Handle to the LLI6 Entry which we need to check. |
1 | - LLI6 Entry is DEAD & can be removed. | |
0 | - LLI6 Entry is not DEAD |
UINT8 LLI6IsRouter | ( | HANDLE | hLLI6 | ) |
Description
The function verifies if the LLI6 Entry belongs to a ROUTER or HOST.
This is for *internal* NDK Stack Usage.
[in] | hLLI6 | Handle to the LLI6 Entry which we need to verify. |
1 | - LLI6 Entry belongs to a ROUTER | |
0 | - LLI6 Entry belongs to a HOST |
UINT8 LLI6IsValid | ( | HANDLE | hLLI6 | ) |
Description
The function checks if the LLI6 Entry is VALID or not? An LLI6 Entry can be used only if it is !INCOMPLETE and its !DEAD
This is for *internal* NDK Stack Usage.
[in] | hLLI6 | Handle to the LLI6 Entry which we need to check. |
1 | - LLI6 Entry is VALID and can be used. | |
0 | - LLI6 Entry is not VALID and should not be used. |
void LLI6Msg | ( | uint | Msg | ) |
Description
Sevices intialization and resource messages for the LLI6 Module.
This is for *internal* NDK Stack Usage.
[in] | Msg | The message event which needs to be handled. |
Not | Applicable. |
HANDLE LLI6New | ( | RT6_ENTRY * | ptr_rt6, | |
UINT8 * | pMacAddress, | |||
UINT8 | IsRouter | |||
) |
Description
This function is used to create a new LLI6 Entry. LLI6 Entries can only be created by the ROUTE6 Module.
This is for *internal* NDK Stack Usage.
[in] | ptr_rt6 | Pointer to the Route6 Entry on which the LLI6 Object is created. |
[in] | pMacAddress | Pointer to the layer2 MAC Address. |
[in] | IsRouter | Flag which indicates if the LLI6 Entry is ROUTER or HOST. This is set to 1 for ROUTER and 0 for HOST. |
Handle | to the new LLI Entry - Success | |
0 | - Error |
void LLI6SetIncomplete | ( | HANDLE | hLLI6 | ) |
Description
The function moves an LLI6 Entry to INCOMPLETE STATE. This API should be used very carefully as it might break the Neighbor Unreachability Detection Logic. This is currently being used from the ROUTE6 Module to handle the special case for the Default Router Selection.
This is for *internal* NDK Stack Usage.
[in] | hLLI6 | Handle to the LLI6 Entry whose status needs to be modified. |
Not | Applicable. |
void LLI6TxIPPacket | ( | PBM_Pkt * | pPkt, | |
HANDLE | hLLI6, | |||
NETIF_DEVICE * | ptr_device, | |||
IP6N | Address | |||
) |
Description
This function is called from the IPv6 stack to resolve the IPv6 address to a corresponding MAC address and push the packet to the drivers.
This is for *internal* NDK Stack Usage.
[in] | pPkt | Pointer to the packet which needs to be transmitted. |
[in] | hLLI6 | Handle to the LLI6 Entry. |
[in] | ptr_device | Pointer to the Network Interface Object on which the packet needs to be sent out. |
[in] | Address | The Destination Address of the packet. |
Not | Applicable. |
void LLI6Update | ( | HANDLE | hLLI6, | |
UINT8 * | mac_address, | |||
UINT32 | RxPktType, | |||
UINT32 | Flags | |||
) |
Description
The function is used to update the LLI6 Entry. This is called whenever one of the Neighbour Discovery packets are received:- a) NS b) NA c) RS d) RA e) Redirect. The function executes the Neighbor Unreachability Detection and Is Router State Machine.
This is for *internal* NDK Stack Usage.
[in] | hLLI6 | Handle to the LLI6 Entry being updated. |
[in] | mac_address | MAC Address which needs to be updated. This can be NULL in which case only the IsRouterStateMachine is executed; the Neighbor Unreachability State Machine is bypassed. |
[in] | RxPktType | The packet type received which has triggered a call to this function. |
[in] | Flags | The flags field in the NA Header received. 0 for all other packets. |
Not | Applicable. |