CC26xx Driver Library
ddi.h
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: ddi.h
3 * Revised: 2015-07-16 12:12:04 +0200 (Thu, 16 Jul 2015)
4 * Revision: 44151
5 *
6 * Description: Defines and prototypes for the DDI master interface.
7 *
8 * Copyright (c) 2015, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 //*****************************************************************************
40 //
45 //
46 //*****************************************************************************
47 
48 #ifndef __DDI_H__
49 #define __DDI_H__
50 
51 //*****************************************************************************
52 //
53 // If building with a C++ compiler, make all of the definitions in this header
54 // have a C binding.
55 //
56 //*****************************************************************************
57 #ifdef __cplusplus
58 extern "C"
59 {
60 #endif
61 
62 #include <stdbool.h>
63 #include <stdint.h>
64 #include <inc/hw_types.h>
65 #include <inc/hw_memmap.h>
66 #include <inc/hw_ddi.h>
67 #include <inc/hw_aux_smph.h>
68 #include <driverlib/debug.h>
69 #include <driverlib/cpu.h>
70 
71 //*****************************************************************************
72 //
73 // Support for DriverLib in ROM:
74 // This section renames all functions that are not "static inline", so that
75 // calling these functions will default to implementation in flash. At the end
76 // of this file a second renaming will change the defaults to implementation in
77 // ROM for available functions.
78 //
79 // To force use of the implementation in flash, e.g. for debugging:
80 // - Globally: Define DRIVERLIB_NOROM at project level
81 // - Per function: Use prefix "NOROM_" when calling the function
82 //
83 //*****************************************************************************
84 #if !defined(DOXYGEN)
85  #define DDI16BitWrite NOROM_DDI16BitWrite
86  #define DDI16BitfieldWrite NOROM_DDI16BitfieldWrite
87  #define DDI16BitRead NOROM_DDI16BitRead
88  #define DDI16BitfieldRead NOROM_DDI16BitfieldRead
89 #endif
90 
91 //*****************************************************************************
92 //
93 // Number of register in the DDI slave
94 //
95 //*****************************************************************************
96 #define DDI_SLAVE_REGS 64
97 
98 
99 //*****************************************************************************
100 //
101 // Defines that is used to control the ADI slave and master
102 //
103 //*****************************************************************************
104 #define DDI_PROTECT 0x00000080
105 #define DDI_ACK 0x00000001
106 #define DDI_SYNC 0x00000000
107 
108 //*****************************************************************************
109 //
110 // API Functions and prototypes
111 //
112 //*****************************************************************************
113 
114 
115 //*****************************************************************************
116 //
117 // Helper functions
118 //
119 //*****************************************************************************
120 
121 //*****************************************************************************
122 //
133 //
134 //*****************************************************************************
135 __STATIC_INLINE void
136 AuxAdiDdiSafeWrite(uint32_t nAddr, uint32_t nData, uint32_t nSize)
137 {
138  // Disable interrupts and remember whether to re-enable
139  bool bIrqEnabled = !CPUcpsid();
140  // Acquire semaphore for accessing ADI/DDI in AUX, perform access, release semaphore
141  while (!HWREG(AUX_SMPH_BASE + AUX_SMPH_O_SMPH0));
142  switch (nSize) {
143  case 1: HWREGB(nAddr) = (uint8_t)nData; break;
144  case 2: HWREGH(nAddr) = (uint16_t)nData; break;
145  case 4: default: HWREG(nAddr) = nData; break;
146  }
147  HWREG(AUX_SMPH_BASE + AUX_SMPH_O_SMPH0) = 1;
148  // Restore interrupt enable
149  if (bIrqEnabled) {
150  CPUcpsie();
151  }
152 }
153 
154 //*****************************************************************************
155 //
165 //
166 //*****************************************************************************
167 __STATIC_INLINE uint32_t
168 AuxAdiDdiSafeRead(uint32_t nAddr, uint32_t nSize)
169 {
170  uint32_t nRet;
171  // Disable interrupts and remember whether to re-enable
172  bool bIrqEnabled = !CPUcpsid();
173  // Acquire semaphore for accessing ADI/DDI in AUX, perform access, release semaphore
174  while (!HWREG(AUX_SMPH_BASE + AUX_SMPH_O_SMPH0));
175  switch (nSize) {
176  case 1: nRet = HWREGB(nAddr); break;
177  case 2: nRet = HWREGH(nAddr); break;
178  case 4: default: nRet = HWREG(nAddr); break;
179  }
180  HWREG(AUX_SMPH_BASE + AUX_SMPH_O_SMPH0) = 1;
181  // Restore interrupt enable
182  if (bIrqEnabled) {
183  CPUcpsie();
184  }
185  return nRet;
186 }
187 
188 #ifdef DRIVERLIB_DEBUG
189 //*****************************************************************************
190 //
203 //
204 //*****************************************************************************
205 static bool
206 DDIBaseValid(uint32_t ui32Base)
207 {
208  return(ui32Base == AUX_DDI0_OSC_BASE);
209 }
210 #endif
211 
212 
213 //*****************************************************************************
214 //
232 //
233 //*****************************************************************************
234 __STATIC_INLINE void
235 DDI32RegWrite(uint32_t ui32Base, uint32_t ui32Reg,
236  uint32_t ui32Val)
237 {
238  //
239  // Check the arguments.
240  //
241  ASSERT(DDIBaseValid(ui32Base));
242  ASSERT(ui32Reg < DDI_SLAVE_REGS);
243 
244  //
245  // Write the value to the register.
246  //
247  AuxAdiDdiSafeWrite(ui32Base + ui32Reg, ui32Val, 4);
248 }
249 
250 //*****************************************************************************
251 //
264 //
265 //*****************************************************************************
266 __STATIC_INLINE uint32_t
267 DDI32RegRead(uint32_t ui32Base, uint32_t ui32Reg)
268 {
269  //
270  // Check the arguments.
271  //
272  ASSERT(DDIBaseValid(ui32Base));
273  ASSERT(ui32Reg < DDI_SLAVE_REGS);
274 
275  //
276  // Read the register and return the value.
277  //
278  return AuxAdiDdiSafeRead(ui32Base + ui32Reg, 4);
279 }
280 
281 //*****************************************************************************
282 //
301 //
302 //*****************************************************************************
303 __STATIC_INLINE void
304 DDI32BitsSet(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
305 {
306  uint32_t ui32RegOffset;
307 
308  //
309  // Check the arguments.
310  //
311  ASSERT(DDIBaseValid(ui32Base));
312  ASSERT(ui32Reg < DDI_SLAVE_REGS);
313 
314  //
315  // Get the correct address of the first register used for setting bits
316  // in the DDI slave.
317  //
318  ui32RegOffset = DDI_O_SET;
319 
320  //
321  // Set the selected bits.
322  //
323  AuxAdiDdiSafeWrite(ui32Base + ui32RegOffset + ui32Reg, ui32Val, 4);
324 }
325 
326 //*****************************************************************************
327 //
341 //
342 //*****************************************************************************
343 __STATIC_INLINE void
344 DDI32BitsClear(uint32_t ui32Base, uint32_t ui32Reg,
345  uint32_t ui32Val)
346 {
347  uint32_t ui32RegOffset;
348 
349  //
350  // Check the arguments.
351  //
352  ASSERT(DDIBaseValid(ui32Base));
353  ASSERT(ui32Reg < DDI_SLAVE_REGS);
354 
355  //
356  // Get the correct address of the first register used for setting bits
357  // in the DDI slave.
358  //
359  ui32RegOffset = DDI_O_CLR;
360 
361  //
362  // Clear the selected bits.
363  //
364  AuxAdiDdiSafeWrite(ui32Base + ui32RegOffset + ui32Reg, ui32Val, 4);
365 }
366 
367 //*****************************************************************************
368 //
392 //
393 //*****************************************************************************
394 __STATIC_INLINE void
395 DDI8SetValBit(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Byte,
396  uint16_t ui16Mask, uint16_t ui16Val)
397 {
398  uint32_t ui32RegOffset;
399 
400  //
401  // Check the arguments.
402  //
403  ASSERT(DDIBaseValid(ui32Base));
404  ASSERT(ui32Reg < DDI_SLAVE_REGS);
405  ASSERT(!(ui16Val & 0xFF00));
406  ASSERT(!(ui16Mask & 0xFF00));
407 
408  //
409  // Get the correct address of the first register used for setting bits
410  // in the DDI slave.
411  //
412  ui32RegOffset = DDI_O_MASK8B + (ui32Reg << 1) + (ui32Byte << 1);
413 
414  //
415  // Set the selected bits.
416  //
417  AuxAdiDdiSafeWrite(ui32Base + ui32RegOffset, (ui16Mask << 8) | ui16Val, 2);
418 }
419 
420 //*****************************************************************************
421 //
445 //
446 //*****************************************************************************
447 __STATIC_INLINE void
448 DDI16SetValBit(uint32_t ui32Base, uint32_t ui32Reg, bool bWriteHigh,
449  uint32_t ui32Mask, uint32_t ui32Val)
450 {
451  uint32_t ui32RegOffset;
452 
453  //
454  // Check the arguments.
455  //
456  ASSERT(DDIBaseValid(ui32Base));
457  ASSERT(ui32Reg < DDI_SLAVE_REGS);
458  ASSERT(!(ui32Val & 0xFFFF0000));
459  ASSERT(!(ui32Mask & 0xFFFF0000));
460 
461  //
462  // Get the correct address of the first register used for setting bits
463  // in the DDI slave.
464  //
465  ui32RegOffset = DDI_O_MASK16B + (ui32Reg << 1) + (bWriteHigh ? 4 : 0);
466 
467  //
468  // Set the selected bits.
469  //
470  AuxAdiDdiSafeWrite(ui32Base + ui32RegOffset, (ui32Mask << 16) | ui32Val, 4);
471 }
472 
473 //*****************************************************************************
474 //
490 //
491 //*****************************************************************************
492 extern void DDI16BitWrite(uint32_t ui32Base, uint32_t ui32Reg,
493  uint32_t ui32Mask, uint32_t ui32WrData);
494 
495 
496 //*****************************************************************************
497 //
513 //
514 //*****************************************************************************
515 extern void DDI16BitfieldWrite(uint32_t ui32Base, uint32_t ui32Reg,
516  uint32_t ui32Mask, uint32_t ui32Shift,
517  uint16_t ui32Data);
518 
519 //*****************************************************************************
520 //
531 //
532 //*****************************************************************************
533 extern uint16_t DDI16BitRead(uint32_t ui32Base, uint32_t ui32Reg,
534  uint32_t ui32Mask);
535 
536 //*****************************************************************************
537 //
552 //
553 //*****************************************************************************
554 extern uint16_t DDI16BitfieldRead(uint32_t ui32Base, uint32_t ui32Reg,
555  uint32_t ui32Mask, uint32_t ui32Shift);
556 
557 //*****************************************************************************
558 //
559 // Support for DriverLib in ROM:
560 // Redirect to implementation in ROM when available.
561 //
562 //*****************************************************************************
563 #if !defined(DRIVERLIB_NOROM) && !defined(DOXYGEN)
564  #include <driverlib/rom.h>
565  #ifdef ROM_DDI16BitWrite
566  #undef DDI16BitWrite
567  #define DDI16BitWrite ROM_DDI16BitWrite
568  #endif
569  #ifdef ROM_DDI16BitfieldWrite
570  #undef DDI16BitfieldWrite
571  #define DDI16BitfieldWrite ROM_DDI16BitfieldWrite
572  #endif
573  #ifdef ROM_DDI16BitRead
574  #undef DDI16BitRead
575  #define DDI16BitRead ROM_DDI16BitRead
576  #endif
577  #ifdef ROM_DDI16BitfieldRead
578  #undef DDI16BitfieldRead
579  #define DDI16BitfieldRead ROM_DDI16BitfieldRead
580  #endif
581 #endif
582 
583 //*****************************************************************************
584 //
585 // Mark the end of the C bindings section for C++ compilers.
586 //
587 //*****************************************************************************
588 #ifdef __cplusplus
589 }
590 #endif
591 
592 #endif // __DDI_H__
593 
594 //*****************************************************************************
595 //
599 //
600 //*****************************************************************************
static void DDI8SetValBit(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Byte, uint16_t ui16Mask, uint16_t ui16Val)
Set a value on any 8 bits inside a 32 bit register in the DDI slave.
Definition: ddi.h:395
void DDI16BitWrite(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32WrData)
Write a single bit using a 16-bit maskable write.
Definition: ddi.c:64
static void DDI32BitsSet(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
Set specific bits in a DDI slave register.
Definition: ddi.h:304
static void DDI32RegWrite(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
Write a 32 bit value to a register in the DDI slave.
Definition: ddi.h:235
static uint32_t AuxAdiDdiSafeRead(uint32_t nAddr, uint32_t nSize)
Safely read from AUX ADI/DDI interfaces using a semaphore.
Definition: ddi.h:168
uint16_t DDI16BitRead(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask)
Read a bit via the DDI using 16-bit read.
Definition: ddi.c:152
void DDI16BitfieldWrite(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32Shift, uint16_t ui32Data)
Write a bit field via the DDI using 16-bit maskable write.
Definition: ddi.c:108
uint16_t DDI16BitfieldRead(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32Shift)
Read a bitfield via the DDI using 16-bit read.
Definition: ddi.c:198
#define ASSERT(expr)
Definition: debug.h:74
uint32_t CPUcpsid(void)
Disable all external interrupts.
Definition: cpu.c:97
static void DDI16SetValBit(uint32_t ui32Base, uint32_t ui32Reg, bool bWriteHigh, uint32_t ui32Mask, uint32_t ui32Val)
Set a value on any 16 bits inside a 32 bit register aligned on a half-word boundary in the DDI slave...
Definition: ddi.h:448
static uint32_t DDI32RegRead(uint32_t ui32Base, uint32_t ui32Reg)
Read the value in a 32 bit register.
Definition: ddi.h:267
uint32_t CPUcpsie(void)
Enable all external interrupts.
Definition: cpu.c:249
static void DDI32BitsClear(uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
Clear specific bits in a 32 bit DDI register.
Definition: ddi.h:344
#define DDI_SLAVE_REGS
Definition: ddi.h:96
static void AuxAdiDdiSafeWrite(uint32_t nAddr, uint32_t nData, uint32_t nSize)
Safely write to AUX ADI/DDI interfaces using a semaphore.
Definition: ddi.h:136