CC26xx Driver Library
cpu.c
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: cpu.c
3 * Revised: 2016-01-06 15:55:48 +0100 (Wed, 06 Jan 2016)
4 * Revision: 45385
5 *
6 * Description: Instruction wrappers for special CPU instructions needed by
7 * the drivers.
8 *
9 * Copyright (c) 2015, Texas Instruments Incorporated
10 * All rights reserved.
11 *
12 * Redistribution and use in source and binary forms, with or without
13 * modification, are permitted provided that the following conditions are met:
14 *
15 * 1) Redistributions of source code must retain the above copyright notice,
16 * this list of conditions and the following disclaimer.
17 *
18 * 2) Redistributions in binary form must reproduce the above copyright notice,
19 * this list of conditions and the following disclaimer in the documentation
20 * and/or other materials provided with the distribution.
21 *
22 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
23 * be used to endorse or promote products derived from this software without
24 * specific prior written permission.
25 *
26 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
27 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
28 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
29 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
30 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
31 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
32 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
33 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
34 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
35 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
36 * POSSIBILITY OF SUCH DAMAGE.
37 *
38 ******************************************************************************/
39 
40 #include <driverlib/cpu.h>
41 
42 //*****************************************************************************
43 //
44 // Handle support for DriverLib in ROM:
45 // This section will undo prototype renaming made in the header file
46 //
47 //*****************************************************************************
48 #if !defined(DOXYGEN)
49  #undef CPUcpsid
50  #define CPUcpsid NOROM_CPUcpsid
51  #undef CPUprimask
52  #define CPUprimask NOROM_CPUprimask
53  #undef CPUcpsie
54  #define CPUcpsie NOROM_CPUcpsie
55  #undef CPUbasepriGet
56  #define CPUbasepriGet NOROM_CPUbasepriGet
57  #undef CPUdelay
58  #define CPUdelay NOROM_CPUdelay
59 #endif
60 
61 //*****************************************************************************
62 //
64 //
65 //*****************************************************************************
66 #if defined(__IAR_SYSTEMS_ICC__)
67 uint32_t
68 CPUcpsid(void)
69 {
70  //
71  // Read PRIMASK and disable interrupts.
72  //
73  __asm(" mrs r0, PRIMASK\n"
74  " cpsid i\n");
75 
76  //
77  // "Warning[Pe940]: missing return statement at end of non-void function"
78  // is suppressed here to avoid putting a "bx lr" in the inline assembly
79  // above and a superfluous return statement here.
80  //
81 #pragma diag_suppress=Pe940
82 }
83 #pragma diag_default=Pe940
84 #elif defined(__CC_ARM) || defined(__ARMCC_VERSION)
85 __asm uint32_t
86 CPUcpsid(void)
87 {
88  //
89  // Read PRIMASK and disable interrupts.
90  //
91  mrs r0, PRIMASK;
92  cpsid i;
93  bx lr
94 }
95 #elif defined(__TI_COMPILER_VERSION__) || defined(DOXYGEN)
96 uint32_t
97 CPUcpsid(void)
98 {
99  //
100  // Read PRIMASK and disable interrupts.
101  //
102  __asm(" mrs r0, PRIMASK\n"
103  " cpsid i\n"
104  " bx lr\n");
105 
106  //
107  // The following keeps the compiler happy, because it wants to see a
108  // return value from this function. It will generate code to return
109  // a zero. However, the real return is the "bx lr" above, so the
110  // return(0) is never executed and the function returns with the value
111  // you expect in R0.
112  //
113  return(0);
114 }
115 #else
116 uint32_t __attribute__((naked))
117 CPUcpsid(void)
118 {
119  uint32_t ui32Ret;
120 
121  //
122  // Read PRIMASK and disable interrupts
123  //
124  __asm(" mrs r0, PRIMASK\n"
125  " cpsid i\n"
126  " bx lr\n"
127  : "=r"(ui32Ret));
128 
129  //
130  // The return is handled in the inline assembly, but the compiler will
131  // still complain if there is not an explicit return here (despite the fact
132  // that this does not result in any code being produced because of the
133  // naked attribute).
134  //
135  return(ui32Ret);
136 }
137 #endif
138 
139 //*****************************************************************************
140 //
142 //
143 //*****************************************************************************
144 #if defined(__IAR_SYSTEMS_ICC__)
145 uint32_t
146 CPUprimask(void)
147 {
148  //
149  // Read PRIMASK.
150  //
151  __asm(" mrs r0, PRIMASK\n");
152 
153  //
154  // "Warning[Pe940]: missing return statement at end of non-void function"
155  // is suppressed here to avoid putting a "bx lr" in the inline assembly
156  // above and a superfluous return statement here.
157  //
158 #pragma diag_suppress=Pe940
159 }
160 #pragma diag_default=Pe940
161 #elif defined(__CC_ARM) || defined(__ARMCC_VERSION)
162 __asm uint32_t
163 CPUprimask(void)
164 {
165  //
166  // Read PRIMASK.
167  //
168  mrs r0, PRIMASK;
169  bx lr
170 }
171 #elif defined(__TI_COMPILER_VERSION__) || defined(DOXYGEN)
172 uint32_t
174 {
175  //
176  // Read PRIMASK.
177  //
178  __asm(" mrs r0, PRIMASK\n"
179  " bx lr\n");
180 
181  //
182  // The following keeps the compiler happy, because it wants to see a
183  // return value from this function. It will generate code to return
184  // a zero. However, the real return is the "bx lr" above, so the
185  // return(0) is never executed and the function returns with the value
186  // you expect in R0.
187  //
188  return(0);
189 }
190 #else
191 uint32_t __attribute__((naked))
192 CPUprimask(void)
193 {
194  uint32_t ui32Ret;
195 
196  //
197  // Read PRIMASK
198  //
199  __asm(" mrs r0, PRIMASK\n"
200  " bx lr\n"
201  : "=r"(ui32Ret));
202 
203  //
204  // The return is handled in the inline assembly, but the compiler will
205  // still complain if there is not an explicit return here (despite the fact
206  // that this does not result in any code being produced because of the
207  // naked attribute).
208  //
209  return(ui32Ret);
210 }
211 #endif
212 
213 //*****************************************************************************
214 //
216 //
217 //*****************************************************************************
218 #if defined(__IAR_SYSTEMS_ICC__)
219 uint32_t
220 CPUcpsie(void)
221 {
222  //
223  // Read PRIMASK and enable interrupts.
224  //
225  __asm(" mrs r0, PRIMASK\n"
226  " cpsie i\n");
227 
228  //
229  // "Warning[Pe940]: missing return statement at end of non-void function"
230  // is suppressed here to avoid putting a "bx lr" in the inline assembly
231  // above and a superfluous return statement here.
232  //
233 #pragma diag_suppress=Pe940
234 }
235 #pragma diag_default=Pe940
236 #elif defined(__CC_ARM) || defined(__ARMCC_VERSION)
237 __asm uint32_t
238 CPUcpsie(void)
239 {
240  //
241  // Read PRIMASK and enable interrupts.
242  //
243  mrs r0, PRIMASK;
244  cpsie i;
245  bx lr
246 }
247 #elif defined(__TI_COMPILER_VERSION__) || defined(DOXYGEN)
248 uint32_t
249 CPUcpsie(void)
250 {
251  //
252  // Read PRIMASK and enable interrupts.
253  //
254  __asm(" mrs r0, PRIMASK\n"
255  " cpsie i\n"
256  " bx lr\n");
257 
258  //
259  // The following keeps the compiler happy, because it wants to see a
260  // return value from this function. It will generate code to return
261  // a zero. However, the real return is the "bx lr" above, so the
262  // return(0) is never executed and the function returns with the value
263  // you expect in R0.
264  //
265  return(0);
266 }
267 #else
268 uint32_t __attribute__((naked))
269 CPUcpsie(void)
270 {
271  uint32_t ui32Ret;
272 
273  //
274  // Read PRIMASK and enable interrupts.
275  //
276  __asm(" mrs r0, PRIMASK\n"
277  " cpsie i\n"
278  " bx lr\n"
279  : "=r"(ui32Ret));
280 
281  //
282  // The return is handled in the inline assembly, but the compiler will
283  // still complain if there is not an explicit return here (despite the fact
284  // that this does not result in any code being produced because of the
285  // naked attribute).
286  //
287  return(ui32Ret);
288 }
289 #endif
290 
291 //*****************************************************************************
292 //
294 //
295 //*****************************************************************************
296 #if defined(__IAR_SYSTEMS_ICC__)
297 uint32_t
298 CPUbasepriGet(void)
299 {
300  //
301  // Read BASEPRI.
302  //
303  __asm(" mrs r0, BASEPRI\n");
304 
305  //
306  // "Warning[Pe940]: missing return statement at end of non-void function"
307  // is suppressed here to avoid putting a "bx lr" in the inline assembly
308  // above and a superfluous return statement here.
309  //
310 #pragma diag_suppress=Pe940
311 }
312 #pragma diag_default=Pe940
313 #elif defined(__CC_ARM) || defined(__ARMCC_VERSION)
314 __asm uint32_t
315 CPUbasepriGet(void)
316 {
317  //
318  // Read BASEPRI.
319  //
320  mrs r0, BASEPRI;
321  bx lr
322 }
323 #elif defined(__TI_COMPILER_VERSION__) || defined(DOXYGEN)
324 uint32_t
326 {
327  //
328  // Read BASEPRI.
329  //
330  __asm(" mrs r0, BASEPRI\n"
331  " bx lr\n");
332 
333  //
334  // The following keeps the compiler happy, because it wants to see a
335  // return value from this function. It will generate code to return
336  // a zero. However, the real return is the "bx lr" above, so the
337  // return(0) is never executed and the function returns with the value
338  // you expect in R0.
339  //
340  return(0);
341 }
342 #else
343 uint32_t __attribute__((naked))
344 CPUbasepriGet(void)
345 {
346  uint32_t ui32Ret;
347 
348  //
349  // Read BASEPRI.
350  //
351  __asm(" mrs r0, BASEPRI\n"
352  " bx lr\n"
353  : "=r"(ui32Ret));
354 
355  //
356  // The return is handled in the inline assembly, but the compiler will
357  // still complain if there is not an explicit return here (despite the fact
358  // that this does not result in any code being produced because of the
359  // naked attribute).
360  //
361  return(ui32Ret);
362 }
363 #endif
364 
365 //*****************************************************************************
366 //
368 //
369 //*****************************************************************************
370 #if defined(__IAR_SYSTEMS_ICC__)
371 void
372 CPUdelay(uint32_t ui32Count)
373 {
374  //
375  // Delay the specified number of times (3 cycles pr. loop)
376  //
377  __asm("CPUdelay:\n"
378  " subs r0, #1\n"
379  " bne.n CPUdelay\n"
380  " bx lr");
381 #pragma diag_suppress=Pe940
382 }
383 #pragma diag_default=Pe940
384 #elif defined(__CC_ARM) || defined(__ARMCC_VERSION)
385 __asm void
386 CPUdelay(uint32_t ui32Count)
387 {
388  //
389  // Delay the specified number of times (3 cycles pr. loop)
390  //
391 CPUdel
392  subs r0, #1;
393  bne CPUdel;
394  bx lr;
395 }
396 #elif defined(__TI_COMPILER_VERSION__) || defined(DOXYGEN)
397 //
398 // For CCS implement this function in pure assembly. This prevents the TI
399 // compiler from doing funny things with the optimizer.
400 //
401  //
402  // Delay the specified number of times (3 cycles pr. loop)
403  //
404 __asm(" .sect \".text:NOROM_CPUdelay\"\n"
405  " .clink\n"
406  " .thumbfunc NOROM_CPUdelay\n"
407  " .thumb\n"
408  " .global NOROM_CPUdelay\n"
409  "NOROM_CPUdelay:\n"
410  " subs r0, #1\n"
411  " bne.n NOROM_CPUdelay\n"
412  " bx lr\n");
413 #else
414 void __attribute__((naked))
415 CPUdelay(uint32_t ui32Count)
416 {
417  //
418  // Delay the specified number of times (3 cycles pr. loop)
419  //
420  __asm(" subs r0, #1\n"
421  " bne NOROM_CPUdelay\n"
422  " bx lr");
423 }
424 #endif
uint32_t CPUprimask(void)
Get the current interrupt state.
Definition: cpu.c:173
uint32_t CPUcpsid(void)
Disable all external interrupts.
Definition: cpu.c:97
__asm(" .sect \".text:NOROM_CPUdelay\"\n"" .clink\n"" .thumbfunc NOROM_CPUdelay\n"" .thumb\n"" .global NOROM_CPUdelay\n""NOROM_CPUdelay:\n"" subs r0, #1\n"" bne.n NOROM_CPUdelay\n"" bx lr\n")
Provide a small delay.
uint32_t CPUcpsie(void)
Enable all external interrupts.
Definition: cpu.c:249
uint32_t CPUbasepriGet(void)
Get the interrupt priority disable level.
Definition: cpu.c:325
void CPUdelay(uint32_t ui32Count)
Provide a small delay.