#include <rf_ble_cmd.h>
Data Fields | |
dataQueue_t * | pRxQ |
dataQueue_t * | pTxQ |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
uint8_t bAutoFlushCrcErr:1 | |
uint8_t bAutoFlushEmpty:1 | |
uint8_t bIncludeLenByte:1 | |
uint8_t bIncludeCrc:1 | |
uint8_t bAppendRssi:1 | |
uint8_t bAppendStatus:1 | |
uint8_t bAppendTimestamp:1 | |
} | rxConfig |
struct { | |
uint8_t lastRxSn:1 | |
uint8_t lastTxSn:1 | |
uint8_t nextTxSn:1 | |
uint8_t bFirstPkt:1 | |
uint8_t bAutoEmpty:1 | |
uint8_t bLlCtrlTx:1 | |
uint8_t bLlCtrlAckRx:1 | |
uint8_t bLlCtrlAckPending:1 | |
} | seqStat |
uint8_t | maxNack |
uint8_t | maxPkt |
uint32_t | accessAddress |
uint32_t | crcInit |
ratmr_t | timeoutTime |
uint16_t | __dummy0 |
uint8_t | __dummy1 |
struct { | |
uint8_t triggerType:4 | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
uint8_t pastTrig:1 | |
} | endTrigger |
ratmr_t | endTime |
Definition at line 490 of file rf_ble_cmd.h.
uint16_t rfCoreHal_bleSlavePar_s::__dummy0 |
Definition at line 518 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::__dummy1 |
Definition at line 519 of file rf_ble_cmd.h.
uint32_t rfCoreHal_bleSlavePar_s::accessAddress |
Definition at line 515 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bAppendRssi |
Definition at line 499 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bAppendStatus |
Definition at line 500 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bAppendTimestamp |
Definition at line 501 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bAutoEmpty |
Definition at line 508 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bAutoFlushCrcErr |
Definition at line 495 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bAutoFlushEmpty |
Definition at line 496 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bAutoFlushIgnored |
Definition at line 494 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bEnaCmd |
Definition at line 522 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bFirstPkt |
Definition at line 507 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bIncludeCrc |
Definition at line 498 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bIncludeLenByte |
Definition at line 497 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bLlCtrlAckPending |
Definition at line 511 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bLlCtrlAckRx |
Definition at line 510 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::bLlCtrlTx |
Definition at line 509 of file rf_ble_cmd.h.
uint32_t rfCoreHal_bleSlavePar_s::crcInit |
Definition at line 516 of file rf_ble_cmd.h.
ratmr_t rfCoreHal_bleSlavePar_s::endTime |
Definition at line 526 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleSlavePar_s::endTrigger |
uint8_t rfCoreHal_bleSlavePar_s::lastRxSn |
Definition at line 504 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::lastTxSn |
Definition at line 505 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::maxNack |
Definition at line 513 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::maxPkt |
Definition at line 514 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::nextTxSn |
Definition at line 506 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::pastTrig |
Definition at line 524 of file rf_ble_cmd.h.
dataQueue_t* rfCoreHal_bleSlavePar_s::pRxQ |
Definition at line 491 of file rf_ble_cmd.h.
dataQueue_t* rfCoreHal_bleSlavePar_s::pTxQ |
Definition at line 492 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleSlavePar_s::rxConfig |
struct { ... } rfCoreHal_bleSlavePar_s::seqStat |
ratmr_t rfCoreHal_bleSlavePar_s::timeoutTime |
Definition at line 517 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::triggerNo |
Definition at line 523 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleSlavePar_s::triggerType |
Definition at line 521 of file rf_ble_cmd.h.