#include <rf_ble_cmd.h>
Data Fields | |
dataQueue_t * | pRxQ |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
uint8_t bAutoFlushCrcErr:1 | |
uint8_t bAutoFlushEmpty:1 | |
uint8_t bIncludeLenByte:1 | |
uint8_t bIncludeCrc:1 | |
uint8_t bAppendRssi:1 | |
uint8_t bAppendStatus:1 | |
uint8_t bAppendTimestamp:1 | |
} | rxConfig |
struct { | |
uint8_t scanFilterPolicy:1 | |
uint8_t bActiveScan:1 | |
uint8_t deviceAddrType:1 | |
uint8_t __pad0__:1 | |
uint8_t bStrictLenFilter:1 | |
uint8_t bAutoWlIgnore:1 | |
uint8_t bEndOnRpt:1 | |
} | scanConfig |
uint16_t | randomState |
uint16_t | backoffCount |
struct { | |
uint8_t logUpperLimit:4 | |
uint8_t bLastSucceeded:1 | |
uint8_t bLastFailed:1 | |
} | backoffPar |
uint8_t | scanReqLen |
uint8_t * | pScanReqData |
uint16_t * | pDeviceAddress |
uint32_t * | pWhiteList |
uint16_t | __dummy0 |
struct { | |
uint8_t triggerType:4 | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
uint8_t pastTrig:1 | |
} | timeoutTrigger |
struct { | |
uint8_t triggerType:4 | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
uint8_t pastTrig:1 | |
} | endTrigger |
ratmr_t | timeoutTime |
ratmr_t | endTime |
Definition at line 572 of file rf_ble_cmd.h.
uint16_t rfCoreHal_bleScannerPar_s::__dummy0 |
Definition at line 604 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::__pad0__ |
Definition at line 588 of file rf_ble_cmd.h.
uint16_t rfCoreHal_bleScannerPar_s::backoffCount |
Definition at line 594 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleScannerPar_s::backoffPar |
uint8_t rfCoreHal_bleScannerPar_s::bActiveScan |
Definition at line 586 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bAppendRssi |
Definition at line 580 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bAppendStatus |
Definition at line 581 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bAppendTimestamp |
Definition at line 582 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bAutoFlushCrcErr |
Definition at line 576 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bAutoFlushEmpty |
Definition at line 577 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bAutoFlushIgnored |
Definition at line 575 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bAutoWlIgnore |
Definition at line 590 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bEnaCmd |
Definition at line 607 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bEndOnRpt |
Definition at line 591 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bIncludeCrc |
Definition at line 579 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bIncludeLenByte |
Definition at line 578 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bLastFailed |
Definition at line 598 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bLastSucceeded |
Definition at line 597 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::bStrictLenFilter |
Definition at line 589 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::deviceAddrType |
Definition at line 587 of file rf_ble_cmd.h.
ratmr_t rfCoreHal_bleScannerPar_s::endTime |
Definition at line 618 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleScannerPar_s::endTrigger |
uint8_t rfCoreHal_bleScannerPar_s::logUpperLimit |
Definition at line 596 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::pastTrig |
Definition at line 609 of file rf_ble_cmd.h.
uint16_t* rfCoreHal_bleScannerPar_s::pDeviceAddress |
Definition at line 602 of file rf_ble_cmd.h.
dataQueue_t* rfCoreHal_bleScannerPar_s::pRxQ |
Definition at line 573 of file rf_ble_cmd.h.
uint8_t* rfCoreHal_bleScannerPar_s::pScanReqData |
Definition at line 601 of file rf_ble_cmd.h.
uint32_t* rfCoreHal_bleScannerPar_s::pWhiteList |
Definition at line 603 of file rf_ble_cmd.h.
uint16_t rfCoreHal_bleScannerPar_s::randomState |
Definition at line 593 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleScannerPar_s::rxConfig |
struct { ... } rfCoreHal_bleScannerPar_s::scanConfig |
uint8_t rfCoreHal_bleScannerPar_s::scanFilterPolicy |
Definition at line 585 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::scanReqLen |
Definition at line 600 of file rf_ble_cmd.h.
ratmr_t rfCoreHal_bleScannerPar_s::timeoutTime |
Definition at line 617 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleScannerPar_s::timeoutTrigger |
uint8_t rfCoreHal_bleScannerPar_s::triggerNo |
Definition at line 608 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleScannerPar_s::triggerType |
Definition at line 606 of file rf_ble_cmd.h.