#include <rf_ble_cmd.h>
Data Fields | |
dataQueue_t * | pRxQ |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
uint8_t bAutoFlushCrcErr:1 | |
uint8_t bAutoFlushEmpty:1 | |
uint8_t bIncludeLenByte:1 | |
uint8_t bIncludeCrc:1 | |
uint8_t bAppendRssi:1 | |
uint8_t bAppendStatus:1 | |
uint8_t bAppendTimestamp:1 | |
} | rxConfig |
struct { | |
uint8_t bUseWhiteList:1 | |
uint8_t bDynamicWinOffset:1 | |
uint8_t deviceAddrType:1 | |
uint8_t peerAddrType:1 | |
uint8_t bStrictLenFilter:1 | |
} | initConfig |
uint8_t | __dummy0 |
uint8_t | connectReqLen |
uint8_t * | pConnectReqData |
uint16_t * | pDeviceAddress |
uint32_t * | pWhiteList |
ratmr_t | connectTime |
uint16_t | __dummy1 |
struct { | |
uint8_t triggerType:4 | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
uint8_t pastTrig:1 | |
} | timeoutTrigger |
struct { | |
uint8_t triggerType:4 | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
uint8_t pastTrig:1 | |
} | endTrigger |
ratmr_t | timeoutTime |
ratmr_t | endTime |
Definition at line 625 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::__dummy0 |
Definition at line 644 of file rf_ble_cmd.h.
uint16_t rfCoreHal_bleInitiatorPar_s::__dummy1 |
Definition at line 650 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bAppendRssi |
Definition at line 633 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bAppendStatus |
Definition at line 634 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bAppendTimestamp |
Definition at line 635 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bAutoFlushCrcErr |
Definition at line 629 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bAutoFlushEmpty |
Definition at line 630 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bAutoFlushIgnored |
Definition at line 628 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bDynamicWinOffset |
Definition at line 639 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bEnaCmd |
Definition at line 653 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bIncludeCrc |
Definition at line 632 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bIncludeLenByte |
Definition at line 631 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bStrictLenFilter |
Definition at line 642 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::bUseWhiteList |
Definition at line 638 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::connectReqLen |
Definition at line 645 of file rf_ble_cmd.h.
ratmr_t rfCoreHal_bleInitiatorPar_s::connectTime |
Definition at line 649 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::deviceAddrType |
Definition at line 640 of file rf_ble_cmd.h.
ratmr_t rfCoreHal_bleInitiatorPar_s::endTime |
Definition at line 664 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleInitiatorPar_s::endTrigger |
struct { ... } rfCoreHal_bleInitiatorPar_s::initConfig |
uint8_t rfCoreHal_bleInitiatorPar_s::pastTrig |
Definition at line 655 of file rf_ble_cmd.h.
uint8_t* rfCoreHal_bleInitiatorPar_s::pConnectReqData |
Definition at line 646 of file rf_ble_cmd.h.
uint16_t* rfCoreHal_bleInitiatorPar_s::pDeviceAddress |
Definition at line 647 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::peerAddrType |
Definition at line 641 of file rf_ble_cmd.h.
dataQueue_t* rfCoreHal_bleInitiatorPar_s::pRxQ |
Definition at line 626 of file rf_ble_cmd.h.
uint32_t* rfCoreHal_bleInitiatorPar_s::pWhiteList |
Definition at line 648 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleInitiatorPar_s::rxConfig |
ratmr_t rfCoreHal_bleInitiatorPar_s::timeoutTime |
Definition at line 663 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleInitiatorPar_s::timeoutTrigger |
uint8_t rfCoreHal_bleInitiatorPar_s::triggerNo |
Definition at line 654 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleInitiatorPar_s::triggerType |
Definition at line 652 of file rf_ble_cmd.h.