#include <rf_ble_cmd.h>
Data Fields | |
dataQueue_t * | pRxQ |
struct { | |
uint8_t bAutoFlushIgnored:1 | |
uint8_t bAutoFlushCrcErr:1 | |
uint8_t bAutoFlushEmpty:1 | |
uint8_t bIncludeLenByte:1 | |
uint8_t bIncludeCrc:1 | |
uint8_t bAppendRssi:1 | |
uint8_t bAppendStatus:1 | |
uint8_t bAppendTimestamp:1 | |
} | rxConfig |
struct { | |
uint8_t advFilterPolicy:2 | |
uint8_t deviceAddrType:1 | |
uint8_t peerAddrType:1 | |
uint8_t bStrictLenFilter:1 | |
} | advConfig |
uint8_t | advLen |
uint8_t | scanRspLen |
uint8_t * | pAdvData |
uint8_t * | pScanRspData |
uint16_t * | pDeviceAddress |
uint32_t * | pWhiteList |
uint16_t | __dummy0 |
uint8_t | __dummy1 |
struct { | |
uint8_t triggerType:4 | |
uint8_t bEnaCmd:1 | |
uint8_t triggerNo:2 | |
uint8_t pastTrig:1 | |
} | endTrigger |
ratmr_t | endTime |
Definition at line 533 of file rf_ble_cmd.h.
uint16_t rfCoreHal_bleAdvPar_s::__dummy0 |
Definition at line 557 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::__dummy1 |
Definition at line 558 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleAdvPar_s::advConfig |
uint8_t rfCoreHal_bleAdvPar_s::advFilterPolicy |
Definition at line 546 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::advLen |
Definition at line 551 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bAppendRssi |
Definition at line 541 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bAppendStatus |
Definition at line 542 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bAppendTimestamp |
Definition at line 543 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bAutoFlushCrcErr |
Definition at line 537 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bAutoFlushEmpty |
Definition at line 538 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bAutoFlushIgnored |
Definition at line 536 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bEnaCmd |
Definition at line 561 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bIncludeCrc |
Definition at line 540 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bIncludeLenByte |
Definition at line 539 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::bStrictLenFilter |
Definition at line 549 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::deviceAddrType |
Definition at line 547 of file rf_ble_cmd.h.
ratmr_t rfCoreHal_bleAdvPar_s::endTime |
Definition at line 565 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleAdvPar_s::endTrigger |
uint8_t* rfCoreHal_bleAdvPar_s::pAdvData |
Definition at line 553 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::pastTrig |
Definition at line 563 of file rf_ble_cmd.h.
uint16_t* rfCoreHal_bleAdvPar_s::pDeviceAddress |
Definition at line 555 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::peerAddrType |
Definition at line 548 of file rf_ble_cmd.h.
dataQueue_t* rfCoreHal_bleAdvPar_s::pRxQ |
Definition at line 534 of file rf_ble_cmd.h.
uint8_t* rfCoreHal_bleAdvPar_s::pScanRspData |
Definition at line 554 of file rf_ble_cmd.h.
uint32_t* rfCoreHal_bleAdvPar_s::pWhiteList |
Definition at line 556 of file rf_ble_cmd.h.
struct { ... } rfCoreHal_bleAdvPar_s::rxConfig |
uint8_t rfCoreHal_bleAdvPar_s::scanRspLen |
Definition at line 552 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::triggerNo |
Definition at line 562 of file rf_ble_cmd.h.
uint8_t rfCoreHal_bleAdvPar_s::triggerType |
Definition at line 560 of file rf_ble_cmd.h.