CC13xx Driver Library
flash.c
Go to the documentation of this file.
1 /******************************************************************************
2 * Filename: flash.c
3 * Revised: 2015-11-02 14:35:00 +0100 (Mon, 02 Nov 2015)
4 * Revision: 44906
5 *
6 * Description: Driver for on chip Flash.
7 *
8 * Copyright (c) 2015, Texas Instruments Incorporated
9 * All rights reserved.
10 *
11 * Redistribution and use in source and binary forms, with or without
12 * modification, are permitted provided that the following conditions are met:
13 *
14 * 1) Redistributions of source code must retain the above copyright notice,
15 * this list of conditions and the following disclaimer.
16 *
17 * 2) Redistributions in binary form must reproduce the above copyright notice,
18 * this list of conditions and the following disclaimer in the documentation
19 * and/or other materials provided with the distribution.
20 *
21 * 3) Neither the name of the ORGANIZATION nor the names of its contributors may
22 * be used to endorse or promote products derived from this software without
23 * specific prior written permission.
24 *
25 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
26 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
27 * IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
28 * ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE
29 * LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
30 * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
31 * SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
32 * INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
33 * CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
34 * ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
35 * POSSIBILITY OF SUCH DAMAGE.
36 *
37 ******************************************************************************/
38 
39 #include <inc/hw_types.h>
40 #include <driverlib/flash.h>
41 #include <driverlib/rom.h>
42 #include <driverlib/chipinfo.h>
43 
44 //*****************************************************************************
45 //
46 // Handle support for DriverLib in ROM:
47 // This section will undo prototype renaming made in the header file
48 //
49 //*****************************************************************************
50 #if !defined(DOXYGEN)
51  #undef FlashPowerModeSet
52  #define FlashPowerModeSet NOROM_FlashPowerModeSet
53  #undef FlashPowerModeGet
54  #define FlashPowerModeGet NOROM_FlashPowerModeGet
55  #undef FlashProtectionSet
56  #define FlashProtectionSet NOROM_FlashProtectionSet
57  #undef FlashProtectionGet
58  #define FlashProtectionGet NOROM_FlashProtectionGet
59  #undef FlashProtectionSave
60  #define FlashProtectionSave NOROM_FlashProtectionSave
61  #undef FlashSectorErase
62  #define FlashSectorErase NOROM_FlashSectorErase
63  #undef FlashProgram
64  #define FlashProgram NOROM_FlashProgram
65  #undef FlashEfuseReadRow
66  #define FlashEfuseReadRow NOROM_FlashEfuseReadRow
67  #undef FlashDisableSectorsForWrite
68  #define FlashDisableSectorsForWrite NOROM_FlashDisableSectorsForWrite
69 #endif
70 
71 //*****************************************************************************
72 //
73 // Default values for security control in customer configuration area in flash
74 // top sector.
75 //
76 //*****************************************************************************
77 const uint8_t g_pui8CcfgDefaultSec[] = {0xFF, 0xFF, 0xFF, 0xC5,
78  0xFF, 0xFF, 0xFF, 0xFF,
79  0xC5, 0xFF, 0xFF, 0xFF,
80  0xC5, 0xC5, 0xC5, 0xFF,
81  0xC5, 0xC5, 0xC5, 0xFF
82  };
83 
84 typedef uint32_t (* FlashPrgPointer_t) (uint8_t *, uint32_t, uint32_t);
85 
86 typedef uint32_t (* FlashSectorErasePointer_t) (uint32_t);
87 
88 //*****************************************************************************
89 //
90 // Function prototypes for static functions
91 //
92 //*****************************************************************************
93 static void SetReadMode(void);
94 
95 //*****************************************************************************
96 //
98 //
99 //*****************************************************************************
100 void
101 FlashPowerModeSet(uint32_t ui32PowerMode, uint32_t ui32BankGracePeriode,
102  uint32_t ui32PumpGracePeriode)
103 {
104  //
105  // Check the arguments.
106  //
107  ASSERT(ui32PowerMode == FLASH_PWR_ACTIVE_MODE ||
108  ui32PowerMode == FLASH_PWR_OFF_MODE ||
109  ui32PowerMode == FLASH_PWR_DEEP_STDBY_MODE);
110  ASSERT(ui32BankGracePeriode <= 0xFF);
111  ASSERT(ui32PumpGracePeriode <= 0xFFFF);
112 
113  switch(ui32PowerMode)
114  {
116  //
117  // Set bank power mode to ACTIVE.
118  //
119  HWREG(FLASH_BASE + FLASH_O_FBFALLBACK) =
120  (HWREG(FLASH_BASE + FLASH_O_FBFALLBACK) &
122 
123  //
124  // Set charge pump power mode to ACTIVE mode.
125  //
126  HWREG(FLASH_BASE + FLASH_O_FPAC1) =
128  break;
129 
130  case FLASH_PWR_OFF_MODE:
131  //
132  // Set bank grace periode.
133  //
134  HWREG(FLASH_BASE + FLASH_O_FBAC) =
135  (HWREG(FLASH_BASE + FLASH_O_FBAC) & (~FLASH_FBAC_BAGP_M)) |
136  ((ui32BankGracePeriode << FLASH_FBAC_BAGP_S) & FLASH_FBAC_BAGP_M);
137 
138  //
139  // Set pump grace periode.
140  //
141  HWREG(FLASH_BASE + FLASH_O_FPAC2) =
143  ((ui32PumpGracePeriode << FLASH_FPAC2_PAGP_S) & FLASH_FPAC2_PAGP_M);
144 
145  //
146  // Set bank power mode to SLEEP.
147  //
149 
150  //
151  // Set charge pump power mode to SLEEP mode.
152  //
154  break;
155 
157  //
158  // Set bank grace periode.
159  //
160  HWREG(FLASH_BASE + FLASH_O_FBAC) =
161  (HWREG(FLASH_BASE + FLASH_O_FBAC) & (~FLASH_FBAC_BAGP_M)) |
162  ((ui32BankGracePeriode << FLASH_FBAC_BAGP_S) & FLASH_FBAC_BAGP_M);
163 
164  //
165  // Set pump grace periode.
166  //
167  HWREG(FLASH_BASE + FLASH_O_FPAC2) =
169  ((ui32PumpGracePeriode << FLASH_FPAC2_PAGP_S) & FLASH_FPAC2_PAGP_M);
170 
171  //
172  // Set bank power mode to DEEP STANDBY mode.
173  //
174  HWREG(FLASH_BASE + FLASH_O_FBFALLBACK) =
175  (HWREG(FLASH_BASE + FLASH_O_FBFALLBACK) &
177 
178  //
179  // Set charge pump power mode to STANDBY mode.
180  //
182  break;
183  }
184 }
185 
186 //*****************************************************************************
187 //
189 //
190 //*****************************************************************************
191 uint32_t
193 {
194  uint32_t ui32PowerMode;
195  uint32_t ui32BankPwrMode;
196 
197  ui32BankPwrMode = HWREG(FLASH_BASE + FLASH_O_FBFALLBACK) &
199 
200  if(ui32BankPwrMode == FBFALLBACK_SLEEP)
201  {
202  ui32PowerMode = FLASH_PWR_OFF_MODE;
203  }
204  else if(ui32BankPwrMode == FBFALLBACK_DEEP_STDBY)
205  {
206  ui32PowerMode = FLASH_PWR_DEEP_STDBY_MODE;
207  }
208  else
209  {
210  ui32PowerMode = FLASH_PWR_ACTIVE_MODE;
211  }
212 
213  //
214  // Return power mode.
215  //
216  return(ui32PowerMode);
217 }
218 
219 //*****************************************************************************
220 //
222 //
223 //*****************************************************************************
224 void
225 FlashProtectionSet(uint32_t ui32SectorAddress, uint32_t ui32ProtectMode)
226 {
227  uint32_t ui32SectorNumber;
228 
229  //
230  // Check the arguments.
231  //
232  ASSERT(ui32SectorAddress <= (FLASHMEM_BASE + FlashSizeGet() -
233  FlashSectorSizeGet()));
234  ASSERT((ui32SectorAddress & (FlashSectorSizeGet() - 1)) == 00);
235 
236  if(ui32ProtectMode == FLASH_WRITE_PROTECT)
237  {
238  ui32SectorNumber = (ui32SectorAddress - FLASHMEM_BASE) /
241 
242  if(ui32SectorNumber <= 31)
243  {
244  HWREG(FLASH_BASE + FLASH_O_FSM_BSLE0) |= (1 << ui32SectorNumber);
245  HWREG(FLASH_BASE + FLASH_O_FSM_BSLP0) |= (1 << ui32SectorNumber);
246  }
247  else if(ui32SectorNumber <= 63)
248  {
249  HWREG(FLASH_BASE + FLASH_O_FSM_BSLE1) |=
250  (1 << (ui32SectorNumber & 0x1F));
251  HWREG(FLASH_BASE + FLASH_O_FSM_BSLP1) |=
252  (1 << (ui32SectorNumber & 0x1F));
253  }
254 
256  }
257 }
258 
259 //*****************************************************************************
260 //
262 //
263 //*****************************************************************************
264 uint32_t
265 FlashProtectionGet(uint32_t ui32SectorAddress)
266 {
267  uint32_t ui32SectorProtect;
268  uint32_t ui32SectorNumber;
269 
270  //
271  // Check the arguments.
272  //
273  ASSERT(ui32SectorAddress <= (FLASHMEM_BASE + FlashSizeGet() -
274  FlashSectorSizeGet()));
275  ASSERT((ui32SectorAddress & (FlashSectorSizeGet() - 1)) == 00);
276 
277  ui32SectorProtect = FLASH_NO_PROTECT;
278  ui32SectorNumber = (ui32SectorAddress - FLASHMEM_BASE) / FlashSectorSizeGet();
279 
280  if(ui32SectorNumber <= 31)
281  {
282  if((HWREG(FLASH_BASE + FLASH_O_FSM_BSLE0) & (1 << ui32SectorNumber)) &&
283  (HWREG(FLASH_BASE + FLASH_O_FSM_BSLP0) & (1 << ui32SectorNumber)))
284  {
285  ui32SectorProtect = FLASH_WRITE_PROTECT;
286  }
287  }
288  else if(ui32SectorNumber <= 63)
289  {
290  if((HWREG(FLASH_BASE + FLASH_O_FSM_BSLE1) &
291  (1 << (ui32SectorNumber & 0x1F))) &&
292  (HWREG(FLASH_BASE + FLASH_O_FSM_BSLP1) &
293  (1 << (ui32SectorNumber & 0x1F))))
294  {
295  ui32SectorProtect = FLASH_WRITE_PROTECT;
296  }
297  }
298 
299  return(ui32SectorProtect);
300 }
301 
302 //*****************************************************************************
303 //
305 //
306 //*****************************************************************************
307 uint32_t
308 FlashProtectionSave(uint32_t ui32SectorAddress)
309 {
310  uint32_t ui32ErrorReturn;
311  uint32_t ui32SectorNumber;
312  uint32_t ui32CcfgSectorAddr;
313  uint32_t ui32ProgBuf;
314 
315  ui32ErrorReturn = FAPI_STATUS_SUCCESS;
316 
317  //
318  // Check the arguments.
319  //
320  ASSERT(ui32SectorAddress <= (FLASHMEM_BASE + FlashSizeGet() -
321  FlashSectorSizeGet()));
322  ASSERT((ui32SectorAddress & (FlashSectorSizeGet() - 1)) == 00);
323 
324  if(FlashProtectionGet(ui32SectorAddress) == FLASH_WRITE_PROTECT)
325  {
326  //
327  // Find sector number for specified sector.
328  //
329  ui32SectorNumber = (ui32SectorAddress - FLASHMEM_BASE) / FlashSectorSizeGet();
330  ui32CcfgSectorAddr = FLASHMEM_BASE + FlashSizeGet() - FlashSectorSizeGet();
331 
332  //
333  // Adjust CCFG address to the 32-bit CCFG word holding the
334  // protect-bit for the specified sector.
335  //
336  ui32CcfgSectorAddr += (((ui32SectorNumber >> 5) * 4) + CCFG_OFFSET_SECT_PROT);
337 
338  //
339  // Find value to program by setting the protect-bit which
340  // corresponds to specified sector number, to 0.
341  // Leave other protect-bits unchanged.
342  //
343  ui32ProgBuf = (~(1 << (ui32SectorNumber & 0x1F))) &
344  *(uint32_t *)ui32CcfgSectorAddr;
345 
346  ui32ErrorReturn = FlashProgram((uint8_t*)&ui32ProgBuf, ui32CcfgSectorAddr,
348  }
349 
350  //
351  // Return status.
352  //
353  return(ui32ErrorReturn);
354 }
355 
356 //*****************************************************************************
357 //
359 //
360 //*****************************************************************************
361 uint32_t
362 FlashSectorErase(uint32_t ui32SectorAddress)
363 {
364  uint32_t ui32ErrorReturn;
365  FlashSectorErasePointer_t FuncPointer;
366 
367  //
368  // Check the arguments.
369  //
370  ASSERT(ui32SectorAddress <= (FLASHMEM_BASE + FlashSizeGet() -
371  FlashSectorSizeGet()));
372  ASSERT((ui32SectorAddress & (FlashSectorSizeGet() - 1)) == 00);
373 
374  //
375  // Call ROM function
376  //
377  FuncPointer = (uint32_t (*)(uint32_t)) (ROM_API_FLASH_TABLE[5]);
378  ui32ErrorReturn = FuncPointer(ui32SectorAddress);
379 
380  //
381  // Enable standby in flash bank since ROM function migth have disabled it
382  //
384 
385  //
386  // Return status of operation.
387  //
388  return(ui32ErrorReturn);
389 
390 }
391 
392 
393 //*****************************************************************************
394 //
396 //
397 //*****************************************************************************
398 uint32_t
399 FlashProgram(uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count)
400 {
401  uint32_t ui32ErrorReturn;
402  FlashPrgPointer_t FuncPointer;
403 
404  //
405  // Check the arguments.
406  //
407  ASSERT((ui32Address + ui32Count) <= (FLASHMEM_BASE + FlashSizeGet()));
408 
409  //
410  // Call ROM function
411  //
412  FuncPointer = (uint32_t (*)(uint8_t *, uint32_t, uint32_t)) (ROM_API_FLASH_TABLE[6]);
413  ui32ErrorReturn = FuncPointer( pui8DataBuffer, ui32Address, ui32Count);
414 
415  //
416  // Enable standby in flash bank since ROM function migth have disabled it
417  //
419 
420  //
421  // Return status of operation.
422  //
423  return(ui32ErrorReturn);
424 
425 }
426 
427 //*****************************************************************************
428 //
430 //
431 //*****************************************************************************
432 bool
433 FlashEfuseReadRow(uint32_t *pui32EfuseData, uint32_t ui32RowAddress)
434 {
435  bool bStatus;
436 
437  //
438  // Make sure the clock for the efuse is enabled
439  //
441 
442  //
443  // Set timing for EFUSE read operations.
444  //
447 
448  //
449  // Clear status register.
450  //
451  HWREG(FLASH_BASE + FLASH_O_EFUSEERROR) = 0;
452 
453  //
454  // Select the FuseROM block 0.
455  //
456  HWREG(FLASH_BASE + FLASH_O_EFUSEADDR) = 0x00000000;
457 
458  //
459  // Start the read operation.
460  //
461  HWREG(FLASH_BASE + FLASH_O_EFUSE) =
463  (ui32RowAddress & FLASH_EFUSE_DUMPWORD_M);
464 
465  //
466  // Wait for operation to finish.
467  //
469  {
470  }
471 
472  //
473  // Check if error reported.
474  //
476  {
477  //
478  // Set error status.
479  //
480  bStatus = 1;
481 
482  //
483  // Clear data.
484  //
485  *pui32EfuseData = 0;
486  }
487  else
488  {
489  //
490  // Set ok status.
491  //
492  bStatus = 0;
493 
494  //
495  // No error. Get data from data register.
496  //
497  *pui32EfuseData = HWREG(FLASH_BASE + FLASH_O_DATALOWER);
498  }
499 
500  //
501  // Disable the efuse clock to conserve power
502  //
504 
505  //
506  // Return the data.
507  //
508  return(bStatus);
509 }
510 
511 
512 //*****************************************************************************
513 //
515 //
516 //*****************************************************************************
517 void
519 {
520  //
521  // Configure flash back to read mode
522  //
523  SetReadMode();
524 
525  //
526  // Disable Level 1 Protection.
527  //
529 
530  //
531  // Disable all sectors for erase and programming.
532  //
533  HWREG(FLASH_BASE + FLASH_O_FBSE) = 0x0000;
534 
535  //
536  // Enable Level 1 Protection.
537  //
538  HWREG(FLASH_BASE + FLASH_O_FBPROT) = 0;
539 
540  //
541  // Protect sectors from sector erase.
542  //
544  HWREG(FLASH_BASE + FLASH_O_FSM_SECTOR1) = 0xFFFFFFFF;
545  HWREG(FLASH_BASE + FLASH_O_FSM_SECTOR2) = 0xFFFFFFFF;
547 }
548 
549 //*****************************************************************************
550 //
558 //
559 //*****************************************************************************
560 static void
562 {
563  uint32_t ui32TrimValue;
564  uint32_t ui32Value;
565 
566  //
567  // Configure the STANDBY_MODE_SEL, STANDBY_PW_SEL, DIS_STANDBY, DIS_IDLE,
568  // VIN_AT_X and VIN_BY_PASS for read mode
569  //
572  {
573  // Select trim values for external regulator mode:
574  // Configure STANDBY_MODE_SEL (OTP offset 0x308 bit 7)
575  // COnfigure STANDBY_PW_SEL (OTP offset 0x308 bit 6:5)
576  // Must be done while the register bit field CONFIG.DIS_STANDBY = 1
578 
579  ui32TrimValue =
580  HWREG(FLASH_CFG_BASE + FCFG1_OFFSET + FCFG1_O_FLASH_OTP_DATA4);
581 
582  ui32Value = ((ui32TrimValue &
586 
587  ui32Value |= ((ui32TrimValue &
591 
592  // Configure DIS_STANDBY (OTP offset 0x308 bit 4).
593  // Configure DIS_IDLE (OTP offset 0x308 bit 3).
594  ui32Value |= ((ui32TrimValue &
599 
600  HWREG(FLASH_BASE + FLASH_O_CFG) = (HWREG(FLASH_BASE + FLASH_O_CFG) &
604  FLASH_CFG_DIS_IDLE_M)) | ui32Value;
605 
606  // Check if sample and hold functionality is disabled.
608  {
609  //
610  // Wait for disabled sample and hold functionality to be stable.
611  //
612  while(!(HWREG(FLASH_BASE + FLASH_O_STAT) & FLASH_STAT_SAMHOLD_DIS))
613  {
614  }
615  }
616 
617  // Configure VIN_AT_X (OTP offset 0x308 bits 2:0)
618  ui32Value = ((ui32TrimValue &
622 
623  // Configure VIN_BY_PASS which is dependent on the VIN_AT_X value.
624  // If VIN_AT_X = 7 then VIN_BY_PASS should be 0 otherwise
625  // VIN_BY_PASS should be 1
626  if(((ui32Value & FLASH_FSEQPMP_VIN_AT_X_M) >>
627  FLASH_FSEQPMP_VIN_AT_X_S) != 0x7)
628  {
629  ui32Value |= FLASH_FSEQPMP_VIN_BY_PASS;
630  }
631 
632  HWREG(FLASH_BASE + FLASH_O_FLOCK) = 0xAAAA;
633  HWREG(FLASH_BASE + FLASH_O_FSEQPMP) =
634  (HWREG(FLASH_BASE + FLASH_O_FSEQPMP) &
636  FLASH_FSEQPMP_VIN_AT_X_M)) | ui32Value;
637  HWREG(FLASH_BASE + FLASH_O_FLOCK) = 0x55AA;
638  }
639  else
640  {
641  // Select trim values for internal regulator mode:
642  // Configure STANDBY_MODE_SEL (OTP offset 0x308 bit 15)
643  // COnfigure STANDBY_PW_SEL (OTP offset 0x308 bit 14:13)
644  // Must be done while the register bit field CONFIG.DIS_STANDBY = 1
646 
647  ui32TrimValue =
648  HWREG(FLASH_CFG_BASE + FCFG1_OFFSET + FCFG1_O_FLASH_OTP_DATA4);
649 
650  ui32Value = ((ui32TrimValue &
654 
655  ui32Value |= ((ui32TrimValue &
659 
660  // Configure DIS_STANDBY (OTP offset 0x308 bit 12).
661  // Configure DIS_IDLE (OTP offset 0x308 bit 11).
662  ui32Value |= ((ui32TrimValue &
667 
668  HWREG(FLASH_BASE + FLASH_O_CFG) = (HWREG(FLASH_BASE + FLASH_O_CFG) &
672  FLASH_CFG_DIS_IDLE_M)) | ui32Value;
673 
674  // Check if sample and hold functionality is disabled.
676  {
677  //
678  // Wait for disabled sample and hold functionality to be stable.
679  //
680  while(!(HWREG(FLASH_BASE + FLASH_O_STAT) & FLASH_STAT_SAMHOLD_DIS))
681  {
682  }
683  }
684 
685  // Configure VIN_AT_X (OTP offset 0x308 bits 10:8)
686  ui32Value = (((ui32TrimValue &
690 
691  // Configure VIN_BY_PASS which is dependent on the VIN_AT_X value.
692  // If VIN_AT_X = 7 then VIN_BY_PASS should be 0 otherwise
693  // VIN_BY_PASS should be 1
694  if(((ui32Value & FLASH_FSEQPMP_VIN_AT_X_M) >>
695  FLASH_FSEQPMP_VIN_AT_X_S) != 0x7)
696  {
697  ui32Value |= FLASH_FSEQPMP_VIN_BY_PASS;
698  }
699 
700  HWREG(FLASH_BASE + FLASH_O_FLOCK) = 0xAAAA;
701  HWREG(FLASH_BASE + FLASH_O_FSEQPMP) =
702  (HWREG(FLASH_BASE + FLASH_O_FSEQPMP) &
704  FLASH_FSEQPMP_VIN_AT_X_M)) | ui32Value;
705  HWREG(FLASH_BASE + FLASH_O_FLOCK) = 0x55AA;
706  }
707 }
708 
709 //*****************************************************************************
710 //
711 // HAPI Flash program function
712 //
713 //*****************************************************************************
714 uint32_t
715 MemBusWrkAroundHapiProgramFlash(uint8_t *pui8DataBuffer, uint32_t ui32Address,
716  uint32_t ui32Count)
717 {
718  uint32_t ui32ErrorReturn;
719  FlashPrgPointer_t FuncPointer;
720  uint32_t ui32RomAddr = HWREG(ROM_HAPI_TABLE_ADDR + (5 * 4));
721 
722  //
723  // Call ROM function
724  //
725  FuncPointer = (uint32_t (*)(uint8_t *, uint32_t, uint32_t)) (ui32RomAddr);
726  ui32ErrorReturn = FuncPointer( pui8DataBuffer, ui32Address, ui32Count);
727 
728  //
729  // Enable standby in flash bank since ROM function migth have disabled it
730  //
732 
733  //
734  // Return status of operation.
735  //
736  return(ui32ErrorReturn);
737 }
738 
739 //*****************************************************************************
740 //
741 // HAPI Flash sector erase function
742 //
743 //*****************************************************************************
744 uint32_t
745 MemBusWrkAroundHapiEraseSector(uint32_t ui32Address)
746 {
747  uint32_t ui32ErrorReturn;
748 
749  FlashSectorErasePointer_t FuncPointer;
750  uint32_t ui32RomAddr = HWREG(ROM_HAPI_TABLE_ADDR + (3 * 4));
751 
752  //
753  // Call ROM function
754  //
755  FuncPointer = (uint32_t (*)(uint32_t)) (ui32RomAddr);
756  ui32ErrorReturn = FuncPointer(ui32Address);
757 
758  //
759  // Enable standby in flash bank since ROM function migth have disabled it
760  //
762 
763  //
764  // Return status of operation.
765  //
766  return(ui32ErrorReturn);
767 }
#define FLASH_PWR_OFF_MODE
Definition: flash.h:125
static uint32_t FlashSectorSizeGet(void)
Get size of a flash sector in number of bytes.
Definition: flash.h:259
#define CCFG_SIZE_SECT_PROT
Definition: flash.h:247
#define DUMPWORD_INSTR
Definition: flash.h:230
#define FBFALLBACK_DEEP_STDBY
Definition: flash.h:192
uint32_t FlashProtectionGet(uint32_t ui32SectorAddress)
Get sector protection.
Definition: flash.c:265
void FlashPowerModeSet(uint32_t ui32PowerMode, uint32_t ui32BankGracePeriode, uint32_t ui32PumpGracePeriode)
Set power mode.
Definition: flash.c:101
void FlashDisableSectorsForWrite(void)
Disables all sectors for erase and programming on the active bank.
Definition: flash.c:518
#define FCFG1_OFFSET
Definition: flash.h:150
uint32_t(* FlashSectorErasePointer_t)(uint32_t)
Definition: flash.c:86
#define FSM_REG_WRT_DISABLE
Definition: flash.h:184
uint32_t FlashPowerModeGet(void)
Get current configured power mode.
Definition: flash.c:192
#define FLASH_NO_PROTECT
Definition: flash.h:134
#define FAPI_STATUS_SUCCESS
Definition: flash.h:103
uint32_t MemBusWrkAroundHapiEraseSector(uint32_t ui32Address)
Definition: flash.c:745
#define FBFALLBACK_SLEEP
Definition: flash.h:191
uint32_t FlashSectorErase(uint32_t ui32SectorAddress)
Erase a flash sector.
Definition: flash.c:362
static uint32_t FlashSizeGet(void)
Get the size of the flash.
Definition: flash.h:283
#define FSM_REG_WRT_ENABLE
Definition: flash.h:183
#define ASSERT(expr)
Definition: debug.h:74
#define FBFALLBACK_ACTIVE
Definition: flash.h:193
bool FlashEfuseReadRow(uint32_t *pui32EfuseData, uint32_t ui32RowAddress)
Reads efuse data from specified row.
Definition: flash.c:433
static void SetReadMode(void)
Definition: flash.c:561
uint32_t MemBusWrkAroundHapiProgramFlash(uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count)
Definition: flash.c:715
#define ROM_HAPI_TABLE_ADDR
Definition: rom.h:61
uint32_t FlashProtectionSave(uint32_t ui32SectorAddress)
Save sector protection to make it permanent.
Definition: flash.c:308
#define FLASH_PWR_ACTIVE_MODE
Definition: flash.h:124
#define FLASH_WRITE_PROTECT
Definition: flash.h:135
#define CCFG_OFFSET_SECT_PROT
Definition: flash.h:245
void FlashProtectionSet(uint32_t ui32SectorAddress, uint32_t ui32ProtectMode)
Set sector protection.
Definition: flash.c:225
#define FLASH_PWR_DEEP_STDBY_MODE
Definition: flash.h:126
uint32_t(* FlashPrgPointer_t)(uint8_t *, uint32_t, uint32_t)
Definition: flash.c:84
#define ROM_API_FLASH_TABLE
Definition: rom.h:250
uint32_t FlashProgram(uint8_t *pui8DataBuffer, uint32_t ui32Address, uint32_t ui32Count)
Programs unprotected main bank flash sectors.
Definition: flash.c:399
const uint8_t g_pui8CcfgDefaultSec[]
Definition: flash.c:77