CC26xx Driver Library

Functions

static bool CCFGRead_EXT_LF_CLK_DIO (void)
 Read EXT_LF_CLK_DIO from CCFG. More...
 
static bool CCFGRead_DIS_GPRAM (void)
 Read DIS_GPRAM from CCFG. More...
 
static uint32_t CCFGRead_SCLK_LF_OPTION (void)
 Read SCLK_LF_OPTION from CCFG. More...
 

Detailed Description

Function Documentation

static bool CCFGRead_DIS_GPRAM ( void  )
inlinestatic

Read DIS_GPRAM from CCFG.

Returns
Value of CCFG field CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM

Definition at line 104 of file ccfgread.h.

static bool CCFGRead_EXT_LF_CLK_DIO ( void  )
inlinestatic

Read EXT_LF_CLK_DIO from CCFG.

Returns
Value of CCFG field CCFG_EXT_LF_CLK_DIO

Definition at line 89 of file ccfgread.h.

static uint32_t CCFGRead_SCLK_LF_OPTION ( void  )
inlinestatic

Read SCLK_LF_OPTION from CCFG.

Returns
Value of CCFG field CCFG_MODE_CONF_SCLK_LF_OPTION. Returns one of the following:

Definition at line 134 of file ccfgread.h.

Macro Definition Documentation

#define SCLK_LF_OPTION_EXTERNAL   1

Definition at line 117 of file ccfgread.h.

#define SCLK_LF_OPTION_RCOSC_LF   3

Definition at line 119 of file ccfgread.h.

#define SCLK_LF_OPTION_XOSC_HF_DLF   0

Definition at line 116 of file ccfgread.h.

#define SCLK_LF_OPTION_XOSC_LF   2

Definition at line 118 of file ccfgread.h.