#include <driverlib/aux_adc.h>
#include <inc/hw_memmap.h>
#include <inc/hw_aux_wuc.h>
#include <inc/hw_fcfg1.h>
#include <driverlib/adi.h>
#include <driverlib/event.h>
Go to the source code of this file.
Functions | |
void | AUXADCDisable (void) |
Disables the ADC. More... | |
void | AUXADCEnableAsync (uint32_t refSource, uint32_t trigger) |
Enables the ADC for asynchronous operation. More... | |
void | AUXADCEnableSync (uint32_t refSource, uint32_t sampleTime, uint32_t trigger) |
Enables the ADC for synchronous operation. More... | |
void | AUXADCDisableInputScaling (void) |
Disables scaling of the ADC input. More... | |
void | AUXADCFlushFifo (void) |
Flushes the ADC FIFO. More... | |
uint32_t | AUXADCReadFifo (void) |
Waits for and returns the first sample in the ADC FIFO. More... | |
uint32_t | AUXADCPopFifo (void) |
Returns the first sample in the ADC FIFO, without waiting. More... | |
int32_t | AUXADCGetAdjustmentGain (uint32_t refSource) |
Returns the gain value used when adjusting for ADC gain/offset. More... | |
int32_t | AUXADCGetAdjustmentOffset (uint32_t refSource) |
Returns the offset value used when adjusting for ADC gain/offset. More... | |
int32_t | AUXADCValueToMicrovolts (int32_t fixedRefVoltage, int32_t adcValue) |
Converts an "adjusted" ADC value to microvolts. More... | |
int32_t | AUXADCMicrovoltsToValue (int32_t fixedRefVoltage, int32_t microvolts) |
Converts a number of microvolts to corresponding "adjusted" ADC value. More... | |
int32_t | AUXADCAdjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset) |
Performs ADC value gain and offset adjustment. More... | |
int32_t | AUXADCUnadjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset) |
Performs the inverse of the ADC value gain and offset adjustment. More... | |