48 #undef AONEventMcuWakeUpSet
49 #define AONEventMcuWakeUpSet NOROM_AONEventMcuWakeUpSet
50 #undef AONEventMcuWakeUpGet
51 #define AONEventMcuWakeUpGet NOROM_AONEventMcuWakeUpGet
52 #undef AONEventAuxWakeUpSet
53 #define AONEventAuxWakeUpSet NOROM_AONEventAuxWakeUpSet
54 #undef AONEventAuxWakeUpGet
55 #define AONEventAuxWakeUpGet NOROM_AONEventAuxWakeUpGet
57 #define AONEventMcuSet NOROM_AONEventMcuSet
59 #define AONEventMcuGet NOROM_AONEventMcuGet
115 uint32_t ui32EventSrc;
202 uint32_t ui32EventSrc;
285 uint32_t ui32EventSrc;
#define AON_EVENT_AUX_WU2
#define AON_EVENT_MCU_WU3
#define AON_EVENT_MCU_WU0
#define AON_EVENT_AUX_WU1
void AONEventMcuWakeUpSet(uint32_t ui32MCUWUEvent, uint32_t ui32EventSrc)
Select event source for the specified MCU wakeup programmable event.
#define AON_EVENT_AUX_WU0
uint32_t AONEventAuxWakeUpGet(uint32_t ui32AUXWUEvent)
Get event source for the specified AUX wakeup programmable event.
#define AON_EVENT_MCU_EVENT2
void AONEventAuxWakeUpSet(uint32_t ui32AUXWUEvent, uint32_t ui32EventSrc)
Select event source for the specified AUX wakeup programmable event.
void AONEventMcuSet(uint32_t ui32MCUEvent, uint32_t ui32EventSrc)
Select event source for the specified programmable event forwarded to the MCU event fabric...
#define AON_EVENT_MCU_EVENT0
#define AON_EVENT_MCU_EVENT1
uint32_t AONEventMcuWakeUpGet(uint32_t ui32MCUWUEvent)
Get event source for the specified MCU wakeup programmable event.
#define AON_EVENT_MCU_WU1
#define AON_EVENT_MCU_WU2
uint32_t AONEventMcuGet(uint32_t ui32MCUEvent)
Get source for the specified programmable event forwarded to the MCU event fabric.