#include <driverlib/aon_event.h>
Go to the source code of this file.
Functions | |
void | AONEventMcuWakeUpSet (uint32_t ui32MCUWUEvent, uint32_t ui32EventSrc) |
Select event source for the specified MCU wakeup programmable event. More... | |
uint32_t | AONEventMcuWakeUpGet (uint32_t ui32MCUWUEvent) |
Get event source for the specified MCU wakeup programmable event. More... | |
void | AONEventAuxWakeUpSet (uint32_t ui32AUXWUEvent, uint32_t ui32EventSrc) |
Select event source for the specified AUX wakeup programmable event. More... | |
uint32_t | AONEventAuxWakeUpGet (uint32_t ui32AUXWUEvent) |
Get event source for the specified AUX wakeup programmable event. More... | |
void | AONEventMcuSet (uint32_t ui32MCUEvent, uint32_t ui32EventSrc) |
Select event source for the specified programmable event forwarded to the MCU event fabric. More... | |
uint32_t | AONEventMcuGet (uint32_t ui32MCUEvent) |
Get source for the specified programmable event forwarded to the MCU event fabric. More... | |