CC13xx Driver Library
rfc.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include <inc/hw_types.h>
#include <inc/hw_memmap.h>
#include <inc/hw_rfc_pwr.h>
#include <inc/hw_rfc_dbell.h>

Go to the source code of this file.

Functions

static void RFCClockEnable (void)
 Enable the RF core clocks. More...
 
static void RFCClockDisable (void)
 Disable the RF core clocks. More...
 
static void RFCCpe0IntEnable (uint32_t ui32Mask)
 Enable CPE0 interrupt. More...
 
static void RFCCpe1IntEnable (uint32_t ui32Mask)
 Enable CPE1 interrupt. More...
 
static void RFCHwIntEnable (uint32_t ui32Mask)
 
static void RFCCpeIntDisable (uint32_t ui32Mask)
 Disable CPE interrupt. More...
 
static void RFCHwIntDisable (uint32_t ui32Mask)
 Disable HW interrupt. More...
 
uint32_t RFCCpeIntGetAndClear (void)
 Get and clear CPE interrupt flags. More...
 
static void RFCCpeIntClear (uint32_t ui32Mask)
 Clear interrupt flags. More...
 
static void RFCHwIntClear (uint32_t ui32Mask)
 Clear interrupt flags. More...
 
static void RFCAckIntClear (void)
 Clear interrupt flags. More...