![]() |
![]() |
|
TI-RTOS for SimpleLink Wireless MCUs
2.14.03.28
|
UARTMSP432 Object. More...
#include <UARTMSP432.h>

Data Fields | |
| struct { | |
| bool opened:1 | |
| UART_Mode readMode:1 | |
| UART_Mode writeMode:1 | |
| UART_DataMode readDataMode:1 | |
| UART_DataMode writeDataMode:1 | |
| UART_ReturnMode readReturnMode:1 | |
| UART_Echo readEcho:1 | |
| bool writeCR:1 | |
| bool bufTimeout:1 | |
| bool callCallback:1 | |
| bool drainByISR:1 | |
| bool rxEnabled:1 | |
| bool txEnabled:1 | |
| } | state |
| HwiP_Handle | hwiHandle |
| ClockP_Handle | timeoutClk |
| uint32_t | baudRate |
| UART_STOP | stopBits |
| UART_PAR | parityType |
| RingBuf_Object | ringBuffer |
| UARTMSP432_FxnSet | readFxns |
| unsigned char * | readBuf |
| size_t | readSize |
| size_t | readCount |
| SemaphoreP_Handle | readSem |
| unsigned int | readTimeout |
| UART_Callback | readCallback |
| const unsigned char * | writeBuf |
| size_t | writeSize |
| size_t | writeCount |
| SemaphoreP_Handle | writeSem |
| unsigned int | writeTimeout |
| UART_Callback | writeCallback |
| unsigned int | writeEmptyClkTimeout |
| Power_NotifyObj | perfChangeNotify |
| uint32_t | perfConstraintMask |
UARTMSP432 Object.
The application must not access any member variables of this structure!
| bool UARTMSP432_Object::opened |
| UART_Mode UARTMSP432_Object::readMode |
| UART_Mode UARTMSP432_Object::writeMode |
| UART_DataMode UARTMSP432_Object::readDataMode |
| UART_DataMode UARTMSP432_Object::writeDataMode |
| UART_ReturnMode UARTMSP432_Object::readReturnMode |
| UART_Echo UARTMSP432_Object::readEcho |
| bool UARTMSP432_Object::writeCR |
| bool UARTMSP432_Object::bufTimeout |
| bool UARTMSP432_Object::callCallback |
| bool UARTMSP432_Object::drainByISR |
| bool UARTMSP432_Object::rxEnabled |
| bool UARTMSP432_Object::txEnabled |
| struct { ... } UARTMSP432_Object::state |
| HwiP_Handle UARTMSP432_Object::hwiHandle |
| ClockP_Handle UARTMSP432_Object::timeoutClk |
| uint32_t UARTMSP432_Object::baudRate |
| UART_STOP UARTMSP432_Object::stopBits |
| UART_PAR UARTMSP432_Object::parityType |
| RingBuf_Object UARTMSP432_Object::ringBuffer |
| UARTMSP432_FxnSet UARTMSP432_Object::readFxns |
| unsigned char* UARTMSP432_Object::readBuf |
| size_t UARTMSP432_Object::readSize |
| size_t UARTMSP432_Object::readCount |
| SemaphoreP_Handle UARTMSP432_Object::readSem |
| unsigned int UARTMSP432_Object::readTimeout |
| UART_Callback UARTMSP432_Object::readCallback |
| const unsigned char* UARTMSP432_Object::writeBuf |
| size_t UARTMSP432_Object::writeSize |
| size_t UARTMSP432_Object::writeCount |
| SemaphoreP_Handle UARTMSP432_Object::writeSem |
| unsigned int UARTMSP432_Object::writeTimeout |
| UART_Callback UARTMSP432_Object::writeCallback |
| unsigned int UARTMSP432_Object::writeEmptyClkTimeout |
| Power_NotifyObj UARTMSP432_Object::perfChangeNotify |
| uint32_t UARTMSP432_Object::perfConstraintMask |