50 #ifndef ti_drivers_sdspi_SDSPIEUSCIA__include
51 #define ti_drivers_sdspi_SDSPIEUSCIA__include
66 #include <ti/sysbios/fatfs/ff.h>
67 #include <ti/sysbios/fatfs/diskio.h>
uint8_t pinSCKModeFunction
Definition: SDSPIEUSCIA.h:145
SDSPIEUSCIA Object.
Definition: SDSPIEUSCIA.h:164
Definition: SDSPIEUSCIA.h:77
The definition of a SDSPI function table that contains the required set of functions to control a spe...
Definition: SDSPI.h:222
uint32_t pinSCK
Definition: SDSPIEUSCIA.h:144
uint32_t pinMOSI
Definition: SDSPIEUSCIA.h:152
uint32_t baseAddr
Definition: SDSPIEUSCIA.h:140
struct SDSPIEUSCIA_Object SDSPIEUSCIA_Object
SDSPIEUSCIA Object.
Definition: SDSPIEUSCIA.h:79
uint32_t pinMISO
Definition: SDSPIEUSCIA.h:148
uint32_t bitRate
Definition: SDSPIEUSCIA.h:168
struct SDSPIEUSCIA_Object * SDSPIEUSCIA_Handle
uint8_t clockSource
Definition: SDSPIEUSCIA.h:141
Definition: SDSPIEUSCIA.h:78
uint8_t portMISO
Definition: SDSPIEUSCIA.h:147
SDSPIEUSCIA_CardType
SD Card type inserted.
Definition: SDSPIEUSCIA.h:75
uint8_t pinMOSIModeFunction
Definition: SDSPIEUSCIA.h:153
FATFS filesystem
Definition: SDSPIEUSCIA.h:169
SDSPIEUSCIA Hardware attributes.
Definition: SDSPIEUSCIA.h:139
uint8_t portCS
Definition: SDSPIEUSCIA.h:155
SDSPIEUSCIA_CardType cardType
Definition: SDSPIEUSCIA.h:167
uint8_t portMOSI
Definition: SDSPIEUSCIA.h:151
uint8_t portSCK
Definition: SDSPIEUSCIA.h:143
DSTATUS diskState
Definition: SDSPIEUSCIA.h:166
struct SDSPIEUSCIA_HWAttrsV1 SDSPIEUSCIA_HWAttrsV1
uint32_t pinCS
Definition: SDSPIEUSCIA.h:156
uint8_t pinMISOModeFunction
Definition: SDSPIEUSCIA.h:149
Definition: SDSPIEUSCIA.h:76
uint16_t driveNumber
Definition: SDSPIEUSCIA.h:165
const SDSPI_FxnTable SDSPIEUSCIA_fxnTable