module ti.sysbios.family.arm.cc26xx.Boot

CC26xx Boot Support

C synopsis target-domain sourced in ti/sysbios/family/arm/cc26xx/Boot.xdc
 
Boot_getBootReason()  // module-wide

Gets the reason for the most recent boot of the CPU

C synopsis target-domain
UInt32 Boot_getBootReason();
 
RETURNS
The reset reason, as reported by the SysCtrlResetSourceGet() DriverLib API.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Boot_Module_id();
// Get this module's unique id
 
Bool Boot_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Boot_Module_heap();
// The heap from which this module allocates memory
 
Bool Boot_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Boot_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Boot_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sysbios/family/arm/cc26xx/Boot.xdc
 
metaonly config Boot.common$  // module-wide

Common module configuration parameters

Configuration settings
Boot.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly config Boot.customerConfig  // module-wide

Include a default customer configuration (CCFG) structure, default is false

Configuration settings
Boot.customerConfig = Bool false;
 
DETAILS
Set to true to link in the default CCFG data structure in driverlib.
 
metaonly config Boot.trimDevice  // module-wide

Trim device flag; determines if trimDevice() is called at boot, default is true

Configuration settings
Boot.trimDevice = Bool true;
 
DETAILS
Set to false to disable trimming of the device during boot.
generated on Tue, 18 Aug 2015 20:38:42 GMT