![]() |
![]() |
TI-RTOS for SimpleLink Wireless MCUs
2.14.02.22
|
MSP432 GPIO driver.
============================================================================
The GPIO header file should be included in an application as follows:
The GPIO module allows you to manage General Purpose I/O pins via simple and portable APIs. The application needs to supply a GPIOMSP432_Config structure to the module (see example below). This structure communicates to the GPIO module how to configure the pins used by the application (See the description of GPIO_PinConfig in the GPIO.h file).
The application is required to call GPIO_init(). This function will initialize all the GPIO pins defined in the GPIO_PinConfig table to the configurations specified. Once completed the other APIs can be used to access the pins.
Asserts are used to verify that the driver has only been initialized, and is reading/writing a valid index.
The following is an example of the code required to use the 2 switches and 4 LEDs on the MSP432 Launchpad board.
Board header:
Board initialization code:
Keep in mind that the callback functions will be called in the context of an interrupt service routine and should be designed accordingly. When an interrupt is triggered, the interrupt status of all (interrupt enabled) pins on a port will be read, cleared, and the respective callbacks will be executed. Callbacks will be called in order from least significant bit to most significant bit.
The GPIO driver interface produces log statements if instrumentation is enabled.
Diagnostics Mask | Log details |
---|---|
Diags_USER1 | basic operations performed |
Go to the source code of this file.
Data Structures | |
struct | GPIOMSP432_Config |
GPIO device specific driver configuration structure. More... | |
Macros | |
#define | GPIOMSP432_EMPTY_PIN 0x0000 |
Device specific port/pin definition macros. More... | |
#define | GPIOMSP432_P1_0 0x101 |
#define | GPIOMSP432_P1_1 0x102 |
#define | GPIOMSP432_P1_2 0x104 |
#define | GPIOMSP432_P1_3 0x108 |
#define | GPIOMSP432_P1_4 0x110 |
#define | GPIOMSP432_P1_5 0x120 |
#define | GPIOMSP432_P1_6 0x140 |
#define | GPIOMSP432_P1_7 0x180 |
#define | GPIOMSP432_P2_0 0x201 |
#define | GPIOMSP432_P2_1 0x202 |
#define | GPIOMSP432_P2_2 0x204 |
#define | GPIOMSP432_P2_3 0x208 |
#define | GPIOMSP432_P2_4 0x210 |
#define | GPIOMSP432_P2_5 0x220 |
#define | GPIOMSP432_P2_6 0x240 |
#define | GPIOMSP432_P2_7 0x280 |
#define | GPIOMSP432_P3_0 0x301 |
#define | GPIOMSP432_P3_1 0x302 |
#define | GPIOMSP432_P3_2 0x304 |
#define | GPIOMSP432_P3_3 0x308 |
#define | GPIOMSP432_P3_4 0x310 |
#define | GPIOMSP432_P3_5 0x320 |
#define | GPIOMSP432_P3_6 0x340 |
#define | GPIOMSP432_P3_7 0x380 |
#define | GPIOMSP432_P4_0 0x401 |
#define | GPIOMSP432_P4_1 0x402 |
#define | GPIOMSP432_P4_2 0x404 |
#define | GPIOMSP432_P4_3 0x408 |
#define | GPIOMSP432_P4_4 0x410 |
#define | GPIOMSP432_P4_5 0x420 |
#define | GPIOMSP432_P4_6 0x440 |
#define | GPIOMSP432_P4_7 0x480 |
#define | GPIOMSP432_P5_0 0x501 |
#define | GPIOMSP432_P5_1 0x502 |
#define | GPIOMSP432_P5_2 0x504 |
#define | GPIOMSP432_P5_3 0x508 |
#define | GPIOMSP432_P5_4 0x510 |
#define | GPIOMSP432_P5_5 0x520 |
#define | GPIOMSP432_P5_6 0x540 |
#define | GPIOMSP432_P5_7 0x580 |
#define | GPIOMSP432_P6_0 0x601 |
#define | GPIOMSP432_P6_1 0x602 |
#define | GPIOMSP432_P6_2 0x604 |
#define | GPIOMSP432_P6_3 0x608 |
#define | GPIOMSP432_P6_4 0x610 |
#define | GPIOMSP432_P6_5 0x620 |
#define | GPIOMSP432_P6_6 0x640 |
#define | GPIOMSP432_P6_7 0x680 |
#define | GPIOMSP432_P7_0 0x701 |
#define | GPIOMSP432_P7_1 0x702 |
#define | GPIOMSP432_P7_2 0x704 |
#define | GPIOMSP432_P7_3 0x708 |
#define | GPIOMSP432_P7_4 0x710 |
#define | GPIOMSP432_P7_5 0x720 |
#define | GPIOMSP432_P7_6 0x740 |
#define | GPIOMSP432_P7_7 0x780 |
#define | GPIOMSP432_P8_0 0x801 |
#define | GPIOMSP432_P8_1 0x802 |
#define | GPIOMSP432_P8_2 0x804 |
#define | GPIOMSP432_P8_3 0x808 |
#define | GPIOMSP432_P8_4 0x810 |
#define | GPIOMSP432_P8_5 0x820 |
#define | GPIOMSP432_P8_6 0x840 |
#define | GPIOMSP432_P8_7 0x880 |
#define | GPIOMSP432_P9_0 0x901 |
#define | GPIOMSP432_P9_1 0x902 |
#define | GPIOMSP432_P9_2 0x904 |
#define | GPIOMSP432_P9_3 0x908 |
#define | GPIOMSP432_P9_4 0x910 |
#define | GPIOMSP432_P9_5 0x920 |
#define | GPIOMSP432_P9_6 0x940 |
#define | GPIOMSP432_P9_7 0x980 |
#define | GPIOMSP432_P10_0 0xa01 |
#define | GPIOMSP432_P10_1 0xa02 |
#define | GPIOMSP432_P10_2 0xa04 |
#define | GPIOMSP432_P10_3 0xa08 |
#define | GPIOMSP432_P10_4 0xa10 |
#define | GPIOMSP432_P10_5 0xa20 |
#define | GPIOMSP432_P10_6 0xa40 |
#define | GPIOMSP432_P10_7 0xa80 |
#define | GPIOMSP432_PJ_0 0xb01 |
#define | GPIOMSP432_PJ_1 0xb02 |
#define | GPIOMSP432_PJ_2 0xb04 |
#define | GPIOMSP432_PJ_3 0xb08 |
#define | GPIOMSP432_PJ_4 0xb10 |
#define | GPIOMSP432_PJ_5 0xb20 |
#define | GPIOMSP432_PJ_6 0xb40 |
#define | GPIOMSP432_PJ_7 0xb80 |
Typedefs | |
typedef struct GPIOMSP432_Config | GPIOMSP432_Config |
GPIO device specific driver configuration structure. More... | |
#define GPIOMSP432_EMPTY_PIN 0x0000 |
Device specific port/pin definition macros.
Below are the port/pin definitions to be used within the board's pin configuration table. These macros should be or'd in with the respective pin configuration settings.
#define GPIOMSP432_P1_0 0x101 |
#define GPIOMSP432_P1_1 0x102 |
#define GPIOMSP432_P1_2 0x104 |
#define GPIOMSP432_P1_3 0x108 |
#define GPIOMSP432_P1_4 0x110 |
#define GPIOMSP432_P1_5 0x120 |
#define GPIOMSP432_P1_6 0x140 |
#define GPIOMSP432_P1_7 0x180 |
#define GPIOMSP432_P2_0 0x201 |
#define GPIOMSP432_P2_1 0x202 |
#define GPIOMSP432_P2_2 0x204 |
#define GPIOMSP432_P2_3 0x208 |
#define GPIOMSP432_P2_4 0x210 |
#define GPIOMSP432_P2_5 0x220 |
#define GPIOMSP432_P2_6 0x240 |
#define GPIOMSP432_P2_7 0x280 |
#define GPIOMSP432_P3_0 0x301 |
#define GPIOMSP432_P3_1 0x302 |
#define GPIOMSP432_P3_2 0x304 |
#define GPIOMSP432_P3_3 0x308 |
#define GPIOMSP432_P3_4 0x310 |
#define GPIOMSP432_P3_5 0x320 |
#define GPIOMSP432_P3_6 0x340 |
#define GPIOMSP432_P3_7 0x380 |
#define GPIOMSP432_P4_0 0x401 |
#define GPIOMSP432_P4_1 0x402 |
#define GPIOMSP432_P4_2 0x404 |
#define GPIOMSP432_P4_3 0x408 |
#define GPIOMSP432_P4_4 0x410 |
#define GPIOMSP432_P4_5 0x420 |
#define GPIOMSP432_P4_6 0x440 |
#define GPIOMSP432_P4_7 0x480 |
#define GPIOMSP432_P5_0 0x501 |
#define GPIOMSP432_P5_1 0x502 |
#define GPIOMSP432_P5_2 0x504 |
#define GPIOMSP432_P5_3 0x508 |
#define GPIOMSP432_P5_4 0x510 |
#define GPIOMSP432_P5_5 0x520 |
#define GPIOMSP432_P5_6 0x540 |
#define GPIOMSP432_P5_7 0x580 |
#define GPIOMSP432_P6_0 0x601 |
#define GPIOMSP432_P6_1 0x602 |
#define GPIOMSP432_P6_2 0x604 |
#define GPIOMSP432_P6_3 0x608 |
#define GPIOMSP432_P6_4 0x610 |
#define GPIOMSP432_P6_5 0x620 |
#define GPIOMSP432_P6_6 0x640 |
#define GPIOMSP432_P6_7 0x680 |
#define GPIOMSP432_P7_0 0x701 |
#define GPIOMSP432_P7_1 0x702 |
#define GPIOMSP432_P7_2 0x704 |
#define GPIOMSP432_P7_3 0x708 |
#define GPIOMSP432_P7_4 0x710 |
#define GPIOMSP432_P7_5 0x720 |
#define GPIOMSP432_P7_6 0x740 |
#define GPIOMSP432_P7_7 0x780 |
#define GPIOMSP432_P8_0 0x801 |
#define GPIOMSP432_P8_1 0x802 |
#define GPIOMSP432_P8_2 0x804 |
#define GPIOMSP432_P8_3 0x808 |
#define GPIOMSP432_P8_4 0x810 |
#define GPIOMSP432_P8_5 0x820 |
#define GPIOMSP432_P8_6 0x840 |
#define GPIOMSP432_P8_7 0x880 |
#define GPIOMSP432_P9_0 0x901 |
#define GPIOMSP432_P9_1 0x902 |
#define GPIOMSP432_P9_2 0x904 |
#define GPIOMSP432_P9_3 0x908 |
#define GPIOMSP432_P9_4 0x910 |
#define GPIOMSP432_P9_5 0x920 |
#define GPIOMSP432_P9_6 0x940 |
#define GPIOMSP432_P9_7 0x980 |
#define GPIOMSP432_P10_0 0xa01 |
#define GPIOMSP432_P10_1 0xa02 |
#define GPIOMSP432_P10_2 0xa04 |
#define GPIOMSP432_P10_3 0xa08 |
#define GPIOMSP432_P10_4 0xa10 |
#define GPIOMSP432_P10_5 0xa20 |
#define GPIOMSP432_P10_6 0xa40 |
#define GPIOMSP432_P10_7 0xa80 |
#define GPIOMSP432_PJ_0 0xb01 |
#define GPIOMSP432_PJ_1 0xb02 |
#define GPIOMSP432_PJ_2 0xb04 |
#define GPIOMSP432_PJ_3 0xb08 |
#define GPIOMSP432_PJ_4 0xb10 |
#define GPIOMSP432_PJ_5 0xb20 |
#define GPIOMSP432_PJ_6 0xb40 |
#define GPIOMSP432_PJ_7 0xb80 |
typedef struct GPIOMSP432_Config GPIOMSP432_Config |
GPIO device specific driver configuration structure.