47 #ifndef ti_drivers_uart_UARTCC3200DMA__include
48 #define ti_drivers_uart_UARTCC3200DMA__include
UART_STOP
UART stop bit settings.
Definition: UART.h:379
unsigned int readTimeout
Definition: UARTCC3200DMA.h:118
UART_Echo readEcho
Definition: UARTCC3200DMA.h:129
Clock interface for the RTOS Porting Interface.
The definition of a UART function table that contains the required set of functions to control a spec...
Definition: UART.h:497
UART_PAR
UART parity type settings.
Definition: UART.h:389
UART_DataMode writeDataMode
Definition: UARTCC3200DMA.h:124
struct UARTCC3200DMA_Object UARTCC3200DMA_Object
UARTCC3200DMA Object.
UART_Mode
UART mode settings.
Definition: UART.h:291
UART_DataMode
UART data mode settings.
Definition: UART.h:339
struct UARTCC3200DMA_HWAttrs UARTCC3200DMA_HWAttrs
UARTCC3200DMA Hardware attributes.
UART_ReturnMode
UART return mode settings.
Definition: UART.h:324
Power_NotifyObj postNotify
Definition: UARTCC3200DMA.h:149
size_t readCount
Definition: UARTCC3200DMA.h:138
UART_Echo
UART echo settings.
Definition: UART.h:357
uint32_t baudRate
Definition: UARTCC3200DMA.h:125
void * SemaphoreP_Handle
Opaque client reference to an instance of a SemaphoreP.
Definition: SemaphoreP.h:96
Semaphore module for the RTOS Porting Interface.
UART_DataMode readDataMode
Definition: UARTCC3200DMA.h:123
ClockP_Handle txFifoEmptyClk
Definition: UARTCC3200DMA.h:148
SemaphoreP_Handle readSem
Definition: UARTCC3200DMA.h:143
size_t writeSize
Definition: UARTCC3200DMA.h:134
void * readBuf
Definition: UARTCC3200DMA.h:137
UART_Mode readMode
Definition: UARTCC3200DMA.h:116
unsigned int intNum
Definition: UARTCC3200DMA.h:99
Power notify object structure.
Definition: Power.h:112
UART_STOP stopBits
Definition: UARTCC3200DMA.h:127
SemaphoreP_Handle writeSem
Definition: UARTCC3200DMA.h:142
UART_LEN dataLength
Definition: UARTCC3200DMA.h:126
unsigned int intPriority
Definition: UARTCC3200DMA.h:101
const UART_FxnTable UARTCC3200DMA_fxnTable
const void * writeBuf
Definition: UARTCC3200DMA.h:132
void(* UART_Callback)(UART_Handle, void *buf, size_t count)
The definition of a callback function used by the UART driver when used in UART_MODE_CALLBACK The cal...
Definition: UART.h:284
UART_PAR parityType
Definition: UARTCC3200DMA.h:128
UARTCC3200DMA Hardware attributes.
Definition: UARTCC3200DMA.h:95
unsigned long rxChannelIndex
Definition: UARTCC3200DMA.h:103
unsigned int writeTimeout
Definition: UARTCC3200DMA.h:119
HwiP_Handle hwiHandle
Definition: UARTCC3200DMA.h:145
unsigned int baseAddr
Definition: UARTCC3200DMA.h:97
size_t readSize
Definition: UARTCC3200DMA.h:139
UART_LEN
UART data length settings.
Definition: UART.h:367
UART_Callback writeCallback
Definition: UARTCC3200DMA.h:121
size_t writeCount
Definition: UARTCC3200DMA.h:133
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
UART_ReturnMode readReturnMode
Definition: UARTCC3200DMA.h:122
UARTCC3200DMA Object.
Definition: UARTCC3200DMA.h:113
struct UARTCC3200DMA_Object * UARTCC3200DMA_Handle
UART_Callback readCallback
Definition: UARTCC3200DMA.h:120
unsigned long txChannelIndex
Definition: UARTCC3200DMA.h:105
Hardware Interrupt module for the RTOS Porting Interface.
bool opened
Definition: UARTCC3200DMA.h:115
UART_Mode writeMode
Definition: UARTCC3200DMA.h:117
void * ClockP_Handle
Opaque client reference to an instance of a ClockP.
Definition: ClockP.h:91