TI-RTOS for SimpleLink Wireless MCUs  2.14.01.20
I2CMSP432.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
48 #ifndef ti_drivers_i2c_I2CMSP432__include
49 #define ti_drivers_i2c_I2CMSP432__include
50 
51 #ifdef __cplusplus
52 extern "C" {
53 #endif
54 
55 #include <stdint.h>
56 #include <stdbool.h>
57 
58 #include <ti/drivers/I2C.h>
59 #include <ti/drivers/ports/HwiP.h>
61 #include <ti/drivers/Power.h>
62 
63 /* I2C function table pointer */
64 extern const I2C_FxnTable I2CMSP432_fxnTable;
65 
72 typedef enum I2CMSP432_Mode {
73  I2CMSP432_IDLE_MODE = 0, /* I2C is not performing a transaction */
74  I2CMSP432_WRITE_MODE, /* I2C is currently performing write operations */
75  I2CMSP432_READ_MODE, /* I2C is currently performing read operations */
76  I2CMSP432_ERROR = 0xFF /* I2C error has occurred, exit gracefully */
78 
97 typedef struct I2CMSP432_HWAttrs {
98  uint32_t baseAddr;
99  uint32_t intNum;
100  uint32_t intPriority;
101  uint8_t clockSource;
103 
109 typedef struct I2CMSP432_Object {
110  SemaphoreP_Handle mutex; /* Grants exclusive access to I2C */
111  SemaphoreP_Handle transferComplete; /* Notify finished I2C transfer */
112 
114 
115  I2C_Transaction *currentTransaction; /* Ptr to current I2C transaction */
116  I2C_CallbackFxn transferCallbackFxn; /* Callback function pointer */
117 
118  /* I2C transaction pointers for I2C_MODE_CALLBACK */
119  I2C_Transaction *headPtr; /* Head ptr for queued transactions */
120  I2C_Transaction *tailPtr; /* Tail ptr for queued transactions */
121 
122  uint8_t *writeBufIdx; /* Internal inc. writeBuf index */
123  size_t writeCountIdx; /* Internal dec. writeCounter */
124 
125  uint8_t *readBufIdx; /* Internal inc. readBuf index */
126  size_t readCountIdx; /* Internal dec. readCounter */
127 
130 
131  volatile I2CMSP432_Mode mode; /* Stores the I2C state */
132  I2C_TransferMode transferMode; /* Blocking or Callback mode */
133  I2C_BitRate bitRate; /* SPI bit rate in Hz */
134  bool isOpen; /* To determine if the SPI is open */
136 
137 #ifdef __cplusplus
138 }
139 #endif
140 
141 #endif /* ti_drivers_i2c_I2CMSP432__include */
I2C_Transaction * currentTransaction
Definition: I2CMSP432.h:115
Definition: I2CMSP432.h:74
I2CMSP432 Object.
Definition: I2CMSP432.h:109
uint32_t baseAddr
Definition: I2CMSP432.h:98
volatile I2CMSP432_Mode mode
Definition: I2CMSP432.h:131
void(* I2C_CallbackFxn)(I2C_Handle, I2C_Transaction *, bool)
I2C callback function.
Definition: I2C.h:248
I2CMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated...
Definition: I2CMSP432.h:97
I2CMSP432_Mode
I2CMSP432 mode.
Definition: I2CMSP432.h:72
SemaphoreP_Handle transferComplete
Definition: I2CMSP432.h:111
I2C_BitRate
I2C bitRate.
Definition: I2C.h:256
Power manager interface.
Definition: I2CMSP432.h:76
const I2C_FxnTable I2CMSP432_fxnTable
I2C_CallbackFxn transferCallbackFxn
Definition: I2CMSP432.h:116
uint8_t * readBufIdx
Definition: I2CMSP432.h:125
struct I2CMSP432_Object I2CMSP432_Object
I2CMSP432 Object.
I2C_TransferMode
I2C transfer mode.
Definition: I2C.h:230
uint32_t intPriority
Definition: I2CMSP432.h:100
void * SemaphoreP_Handle
Opaque client reference to an instance of a SemaphoreP.
Definition: SemaphoreP.h:96
Semaphore module for the RTOS Porting Interface.
The definition of a I2C function table that contains the required set of functions to control a speci...
Definition: I2C.h:328
I2C_Transaction * tailPtr
Definition: I2CMSP432.h:120
Definition: I2CMSP432.h:75
SemaphoreP_Handle mutex
Definition: I2CMSP432.h:110
struct I2CMSP432_HWAttrs I2CMSP432_HWAttrs
I2CMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated...
size_t readCountIdx
Definition: I2CMSP432.h:126
I2C_BitRate bitRate
Definition: I2CMSP432.h:133
Power notify object structure.
Definition: Power.h:112
uint32_t intNum
Definition: I2CMSP432.h:99
I2C_Transaction * headPtr
Definition: I2CMSP432.h:119
Power_NotifyObj perfChangeNotify
Definition: I2CMSP432.h:128
uint8_t * writeBufIdx
Definition: I2CMSP432.h:122
size_t writeCountIdx
Definition: I2CMSP432.h:123
uint32_t perfConstraintMask
Definition: I2CMSP432.h:129
I2C_TransferMode transferMode
Definition: I2CMSP432.h:132
bool isOpen
Definition: I2CMSP432.h:134
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
uint8_t clockSource
Definition: I2CMSP432.h:101
I2C transaction.
Definition: I2C.h:210
Hardware Interrupt module for the RTOS Porting Interface.
Definition: I2CMSP432.h:73
I2C driver interface.
HwiP_Handle hwiHandle
Definition: I2CMSP432.h:113
Copyright 2015, Texas Instruments Incorporated