IPC API
3.10.01.11
|
Example of a host-side module which uses MmRpc to invoke functions on a remote processor.
============================================================================
#include <stddef.h>
#include <stdint.h>
Go to the source code of this file.
Data Structures | |
struct | Mx_Compute |
Compute structure. More... |
Macros | |
#define | Mx_S_SUCCESS (0) |
Operation is successful. | |
#define | Mx_E_FAIL (-1) |
Operation failed. |
Functions | |
int | Mx_initialize (UInt16 procId) |
Initialize the module, must be called first. | |
void | Mx_finalize (void) |
Finalize the module, must be called last. | |
int32_t | Mx_triple (uint32_t a) |
Sample function which multiplies argument by three. | |
int32_t | Mx_add (int32_t a, int32_t b) |
Sample function which addes two arguments. | |
int32_t | Mx_compute_Linux (Mx_Compute *compute, int fd, int fdIn, int fdOut) |
Sample function which has pointer parameter (DMA_BUF) to a structure with two embedded pointers. Linux version. |
#define Mx_S_SUCCESS (0) |
Operation is successful.
#define Mx_E_FAIL (-1) |
Operation failed.
int Mx_initialize | ( | UInt16 | procId | ) |
Initialize the module, must be called first.
void Mx_finalize | ( | void | ) |
Finalize the module, must be called last.
int32_t Mx_triple | ( | uint32_t | a | ) |
Sample function which multiplies argument by three.
int32_t Mx_add | ( | int32_t | a, |
int32_t | b | ||
) |
Sample function which addes two arguments.
int32_t Mx_compute_Linux | ( | Mx_Compute * | compute, |
int | fd, | ||
int | fdIn, | ||
int | fdOut | ||
) |
Sample function which has pointer parameter (DMA_BUF) to a structure with two embedded pointers. Linux version.