![]() |
![]() |
SysLink API Reference
2.21.03.11
|
Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params. More...
#include <SyslinkMemMgr.h>
Data Fields | |
UInt32 | size |
SyslinkMemMgr_Type | memMgrType |
UInt8 | name [32u] |
Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params.
UInt32 SyslinkMemMgr_CreateParams_tag::size |
Size of the param structure
SyslinkMemMgr_Type SyslinkMemMgr_CreateParams_tag::memMgrType |
type of implementation.
UInt8 SyslinkMemMgr_CreateParams_tag::name[32u] |
Name of the instance