SysLink API Reference  2.21.03.11
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Pages
Data Fields
RingIO_sharedMemReqDetails_tag Struct Reference

Structure defining config parameters for opening the RingIO instances. More...

#include <RingIO.h>

Collaboration diagram for RingIO_sharedMemReqDetails_tag:
Collaboration graph

Data Fields

UInt32 ctrlSharedMemReq
UInt32 dataSharedMemReq
UInt32 attrSharedMemReq

Detailed Description

Structure defining config parameters for opening the RingIO instances.


Field Documentation

UInt32 RingIO_sharedMemReqDetails_tag::ctrlSharedMemReq

Instance specific control shared memory requirements

UInt32 RingIO_sharedMemReqDetails_tag::dataSharedMemReq

Data buffer shared memory requirements

UInt32 RingIO_sharedMemReqDetails_tag::attrSharedMemReq

Attribute buffer shared memory requirements


The documentation for this struct was generated from the following file:
Copyright 2014, Texas Instruments Incorporated