SysLink API Reference
2.21.03.11
|
Characteristics of the slave processor. More...
#include <ProcMgr.h>
Data Fields | |
ProcMgr_BootMode | bootMode |
UInt16 | maxMemoryRegions |
UInt16 | numMemEntries |
ProcMgr_MappedMemEntry | memEntries [0] |
Characteristics of the slave processor.
ProcMgr_BootMode ProcMgr_ProcInfo_tag::bootMode |
Boot mode of the processor
UInt16 ProcMgr_ProcInfo_tag::maxMemoryRegions |
Value of ProcMgr_Object.maxMemoryRegions
UInt16 ProcMgr_ProcInfo_tag::numMemEntries |
Number of valid memory entries
ProcMgr_MappedMemEntry ProcMgr_ProcInfo_tag::memEntries[0] |
Configuration of memory regions