![]() |
![]() |
SysLink API Reference
2.21.03.11
|
Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure. More...
#include <FrameQ.h>
Data Fields | |
UInt32 | size |
FrameQ_Interface | ctrlInterfaceType |
String | name |
Bool | openFlag |
Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure.
UInt32 FrameQ_CreateParams_Tag::size |
Size of the paramstructure
FrameQ_Interface FrameQ_CreateParams_Tag::ctrlInterfaceType |
Interface type
String FrameQ_CreateParams_Tag::name |
Name of the instance
Bool FrameQ_CreateParams_Tag::openFlag |