SysLink API Reference
2.21.01.05
|
Argument for the Ipc_CONTROLCMD_SETTERMINATEPOLICY command. More...
#include <IpcHost.h>
Data Fields | |
Int | policy |
Argument for the Ipc_CONTROLCMD_SETTERMINATEPOLICY command.
Initialize a structure of this type with the desired terminate policy. Pass the address of this structure as the arg
parameter to Ipc_control() along with this command type. This must be done before calling the load callback.
Int Ipc_Terminate::policy |
terminate policy