![]() |
![]() |
SysLink API Reference
2.21.01.05
|
Common parameters required to create FrameQBufMgr instance of any implementation. More...
#include <FrameQBufMgr.h>
Data Fields | |
FrameQBufMgr_CreateParams | commonCreateParams |
Ptr | impParams |
UInt32 | impParamsSize |
Common parameters required to create FrameQBufMgr instance of any implementation.
This struct must be the first element of the implementation-specific create params structure.
FrameQBufMgr_CreateParams FrameQBufMgr_Params::commonCreateParams |
Ptr FrameQBufMgr_Params::impParams |
Pointer to implementation-specific struct
UInt32 FrameQBufMgr_Params::impParamsSize |
Size of the implementation-specific impParams
struct.