![]() |
![]() |
SysLink API Reference
2.21.01.05
|
Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure . More...
#include <FrameQ.h>
Data Fields | |
FrameQ_CreateParams | commonCreateParams |
Ptr | impParams |
UInt32 | impParamsSize |
Common parameters required to create FrameQ instance of any implementation. It should be the first element of the actual implementaton params structure .
FrameQ_CreateParams FrameQ_Params::commonCreateParams |
Ptr FrameQ_Params::impParams |
Pointer to implementation specific parameters
UInt32 FrameQ_Params::impParamsSize |
Size of the implementation specific structure pointed by impParams.