SysLink API Reference
2.21.01.05
|
Notification parameter structure. More...
#include <FrameQ.h>
Data Fields | |
FrameQ_NotifyType | notifyType |
UInt32 | watermark |
FrameQ_NotifyFunc | cbFxnPtr |
Ptr | cbContext |
Ptr | cbClientHandle |
Notification parameter structure.
FrameQ_NotifyType FrameQ_NotifyParams_Tag::notifyType |
Notification type
UInt32 FrameQ_NotifyParams_Tag::watermark |
Minumum number of free frames required to generate notification Same water mark for all the individual freeFramePools in the set.
FrameQ_NotifyFunc FrameQ_NotifyParams_Tag::cbFxnPtr |
Cacll back function
Ptr FrameQ_NotifyParams_Tag::cbContext |
Context pointer that needs to be passed to call back function.
Ptr FrameQ_NotifyParams_Tag::cbClientHandle |
Handle that needs to be passed as first arg to call back. Ideally this should be callers client handle.