SysLink API Reference
2.21.00.03
|
Header file implementing Memory manager. It is a wrapper implementation to support Shared memory allocation using heap address translations using shared region or Tiler buffer allocation using tiler buffer manager and address translations.
Go to the source code of this file.
Data Structures | |
struct | SyslinkMemMgr_CreateParams_tag |
Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params. More... | |
struct | SyslinkMemMgr_AllocBlock_tag |
struct | SyslinkMemMgr_AllocParams_tag |
Alloc params. More... |
Macros | |
#define | MEMMGR_MAX_NAME_LENGTH 32u |
#define | MEMMGR_MAX_TILER_BLOCKS 10u |
#define | SyslinkMemMgr_Params SyslinkMemMgr_CreateParams |
Typedefs | |
typedef enum SyslinkMemMgr_Type_Type_tag | SyslinkMemMgr_Type |
enum for denoting the different types of SyslinkMemMgr implementations. | |
typedef struct SyslinkMemMgr_CreateParams_tag | SyslinkMemMgr_CreateParams |
Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params. | |
typedef struct SyslinkMemMgr_AllocBlock_tag | SyslinkMemMgr_AllocBlock |
typedef struct SyslinkMemMgr_AllocParams_tag | SyslinkMemMgr_AllocParams |
Alloc params. | |
typedef struct SyslinkMemMgr_Object | SyslinkMemMgr_Object |
Forward declaration of structure defining object for the MemoryManger. | |
typedef SyslinkMemMgr_Object * | SyslinkMemMgr_Handle |
Handle for the MemoryManager instance. |
Enumerations | |
enum | SyslinkMemMgr_AddrType { SyslinkMemMgr_AddrType_Virtual = 0u, SyslinkMemMgr_AddrType_Portable = 1u, SyslinkMemMgr_AddrType_EndValue = 2u } |
Enumerations to indicate address types used for translation. More... | |
enum | SyslinkMemMgr_Type_Type_tag { SyslinkMemMgr_TYPE_SHAREDMEM = 0x0, SyslinkMemMgr_TYPE_TILERMEM = 0x1 } |
enum for denoting the different types of SyslinkMemMgr implementations. More... |
Functions | |
Int32 | SyslinkMemMgr_setup (Void) |
Int32 | SyslinkMemMgr_destroy (Void) |
SyslinkMemMgr_Handle | SyslinkMemMgr_create (Ptr params) |
Int32 | SyslinkMemMgr_delete (SyslinkMemMgr_Handle *pHandle) |
Ptr | SyslinkMemMgr_alloc (SyslinkMemMgr_Handle handle, SyslinkMemMgr_AllocParams *params) |
Int32 | SyslinkMemMgr_free (SyslinkMemMgr_Handle handle, Ptr ptr, UInt32 size) |
Ptr | SyslinkMemMgr_map (SyslinkMemMgr_Handle handle, Ptr arg) |
Int32 | SyslinkMemMgr_unmap (SyslinkMemMgr_Handle handle, Ptr arg) |
Ptr | SyslinkMemMgr_translate (SyslinkMemMgr_Handle handle, Ptr srcAddr, SyslinkMemMgr_AddrType srcAddrType, SyslinkMemMgr_AddrType desAddrType) |
Ptr | SyslinkMemMgr_getKnlHandle (SyslinkMemMgr_Handle handle) |
#define MEMMGR_MAX_NAME_LENGTH 32u |
#define MEMMGR_MAX_TILER_BLOCKS 10u |
#define SyslinkMemMgr_Params SyslinkMemMgr_CreateParams |
typedef enum SyslinkMemMgr_Type_Type_tag SyslinkMemMgr_Type |
enum for denoting the different types of SyslinkMemMgr implementations.
typedef struct SyslinkMemMgr_CreateParams_tag SyslinkMemMgr_CreateParams |
Structure defining common create parameters for the Memory manager module.Should be the first element in implementation specific create params.
typedef struct SyslinkMemMgr_AllocBlock_tag SyslinkMemMgr_AllocBlock |
typedef struct SyslinkMemMgr_AllocParams_tag SyslinkMemMgr_AllocParams |
Alloc params.
typedef struct SyslinkMemMgr_Object SyslinkMemMgr_Object |
Forward declaration of structure defining object for the MemoryManger.
typedef SyslinkMemMgr_Object* SyslinkMemMgr_Handle |
Handle for the MemoryManager instance.
Enumerations to indicate address types used for translation.
SyslinkMemMgr_Handle SyslinkMemMgr_create | ( | Ptr | params | ) |
Int32 SyslinkMemMgr_delete | ( | SyslinkMemMgr_Handle * | pHandle | ) |
Ptr SyslinkMemMgr_alloc | ( | SyslinkMemMgr_Handle | handle, |
SyslinkMemMgr_AllocParams * | params | ||
) |
Int32 SyslinkMemMgr_free | ( | SyslinkMemMgr_Handle | handle, |
Ptr | ptr, | ||
UInt32 | size | ||
) |
Ptr SyslinkMemMgr_map | ( | SyslinkMemMgr_Handle | handle, |
Ptr | arg | ||
) |
Int32 SyslinkMemMgr_unmap | ( | SyslinkMemMgr_Handle | handle, |
Ptr | arg | ||
) |
Ptr SyslinkMemMgr_translate | ( | SyslinkMemMgr_Handle | handle, |
Ptr | srcAddr, | ||
SyslinkMemMgr_AddrType | srcAddrType, | ||
SyslinkMemMgr_AddrType | desAddrType | ||
) |
Ptr SyslinkMemMgr_getKnlHandle | ( | SyslinkMemMgr_Handle | handle | ) |