![]() |
![]() |
SysLink API Reference
2.21.00.03
|
Memory abstraction APIs for local memory allocation.
This provides a direct access to local memory allocation, which does not require creation of a Heap.
Go to the source code of this file.
Functions | |
Int32 | MemoryOS_setup (void) |
Int32 | MemoryOS_destroy (void) |
Ptr | MemoryOS_alloc (UInt32 size, UInt32 align, UInt32 flags) |
Ptr | MemoryOS_calloc (UInt32 size, UInt32 align, UInt32 flags) |
Void | MemoryOS_free (Ptr ptr, UInt32 size, UInt32 flags) |
Ptr | MemoryOS_copy (Ptr dst, Ptr src, UInt32 len) |
Ptr | MemoryOS_set (Ptr buf, Int value, UInt32 len) |
Ptr | MemoryOS_translate (Ptr srcAddr, Memory_XltFlags flags) |
Int32 MemoryOS_setup | ( | void | ) |
Int32 MemoryOS_destroy | ( | void | ) |