![]() |
![]() |
SysLink API Reference
2.21.00.03
|
Header file for Gate based on Monitor.
Go to the source code of this file.
Macros | |
#define | GateMonitor_E_INVALIDARG -1 |
Argument passed to a function is invalid. | |
#define | GateMonitor_E_MEMORY -2 |
Memory allocation failed. | |
#define | GateMonitor_E_BUSY -3 |
The name is already registered or not. | |
#define | GateMonitor_E_FAIL -4 |
Generic failure. | |
#define | GateMonitor_E_NOTFOUND -5 |
Name not found in the nameserver. | |
#define | GateMonitor_E_INVALIDSTATE -6 |
Module is not initialized. | |
#define | GateMonitor_E_INUSE -7 |
Indicates that the instance is in use. | |
#define | GateMonitor_E_HANDLE -8 |
An invalid handle was provided. | |
#define | GateMonitor_S_SUCCESS 0 |
Operation successful. |
Typedefs | |
typedef struct GateMonitor_Object | GateMonitor_Object |
Object for GateMonitor. | |
typedef GateMonitor_Object * | GateMonitor_Handle |
Handle for GateMonitor. | |
typedef Void | GateMonitor_Params |
Functions | |
GateMonitor_Handle | GateMonitor_create (const GateMonitor_Params *params) |
Int | GateMonitor_delete (GateMonitor_Handle *handle) |
#define GateMonitor_E_INVALIDARG -1 |
Argument passed to a function is invalid.
#define GateMonitor_E_MEMORY -2 |
Memory allocation failed.
#define GateMonitor_E_BUSY -3 |
The name is already registered or not.
#define GateMonitor_E_FAIL -4 |
Generic failure.
#define GateMonitor_E_NOTFOUND -5 |
Name not found in the nameserver.
#define GateMonitor_E_INVALIDSTATE -6 |
Module is not initialized.
#define GateMonitor_E_INUSE -7 |
Indicates that the instance is in use.
#define GateMonitor_E_HANDLE -8 |
An invalid handle was provided.
#define GateMonitor_S_SUCCESS 0 |
Operation successful.
typedef struct GateMonitor_Object GateMonitor_Object |
Object for GateMonitor.
typedef GateMonitor_Object* GateMonitor_Handle |
Handle for GateMonitor.
typedef Void GateMonitor_Params |
No parameters for GateMonitor creation
GateMonitor_Handle GateMonitor_create | ( | const GateMonitor_Params * | params | ) |
Int GateMonitor_delete | ( | GateMonitor_Handle * | handle | ) |